Skip to main content
Visitor II
April 29, 2024
Question

New error without changing the code: "Error in final launch sequence" Please help me

Today I suddenly got a new error message when trying run my project debug:

 

Error in final launch sequence:


Failed to execute MI command:

load C:\\....\\labb3_klockaknapp2\\Debug\\labb3_klockaknapp2.elf


Error message from debugger back end:

Error finishing flash operation

Failed to execute MI command:

load C:\\.....\\labb3_klockaknapp2\\Debug\\labb3_klockaknapp2.elf


Error message from debugger back end:

Error finishing flash operation

Failed to execute MI command:

load C:\\.......\\labb3_klockaknapp2\\Debug\\labb3_klockaknapp2.elf


Error message from debugger back end:

Error finishing flash operation

Error finishing flash operation

I tried creating a new project and transfering code etc, but nothing changed.
The code worked a few days ago.
and the only change i did was moving my 4 number - 7 segment display and it's cables a few steps to the left on the breadboard.

This topic has been closed for replies.

1 reply

ST Technical Moderator
April 30, 2024

Hello @Ambalrith 

Make sure to use the latest version of STM32CubeIDE.

Clean your project and delete the debug folder. Then, try flash the code using STM32CubeProgrammer and update the firmware.

Otherwise, try re-install the CubeIDE.

 
In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks