Skip to main content
Lucky
Associate II
Aug 8, 2019 5:11 PM UTC
Solved

Need Evaluation Kit for this controller STM32L452RCT6 . Is there any alternate Eval Board available?

Actually In our Company the Controller is using STM32L452RCT6 Before Getting A sample Design Board. I need to test with any Eval Board of STM32L4 Series. I Need Evaluation Kit for this controller STM32L4RCT6 Is there any alternate Eval Board available. Hope I am looking forward for your reply.

This topic has been closed for replies.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Aug 9, 2019 1:41 PM UTC

STM32Cube_FW_L4_V1.14.0\Projects\NUCLEO-L452RE\Applications\USB_Device\CDC_Standalone\readme.txt

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

11 replies

Tesla DeLorean
Guru
Aug 8, 2019 6:26 PM UTC

There are several STM32L4R (L4+) boards in EVAL, DISCO and NUCLEO formats. These would likely suffice as proxies, lacking any specific stated requirements.​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Tesla DeLorean
Guru
Aug 8, 2019 7:41 PM UTC
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Lucky
LuckyAuthor
Associate II
Aug 9, 2019 5:23 AM UTC

Hi Clive,

Thank you for your response. As per our requirements the above 3 boards won't suitable , it doesn't have USB device support. The above reference Board support only USB OTG 2.0 FS. I need the Board with USB Device Support. Is it Board Available in Market with USB Device support. Hope I am looking forward for your reply.

Piranha
Principal III
Aug 9, 2019 5:48 AM UTC

First, there is no such a STM32L4RCT6 MCU. Second, how about reading at least first lines in a data sheet?

The devices embed an USB OTG full-speed device/host/OTG peripheral with integrated transceivers. The USB OTG FS peripheral is compliant with the USB 2.0 specification and with the OTG 2.0 specification.

Lucky
LuckyAuthor
Associate II
Aug 9, 2019 6:09 AM UTC

Hi Piranha,

Thank for your response. I am extremely sorry spell mistake STM32L4RCT6 MCU instead of STM32L452RCT6 MCU.

Actually, I am asking instead of a USB OTG full speed ,is it directly USB FS Device mounted on PCB Eval Board available or not.

Tesla DeLorean
Guru
Aug 9, 2019 11:18 AM UTC

Pretty sure these can be HOST or DEVICE, if that's what the question is. Look at board code examples in CubeL4.

​

Edit suggests a non L4+ device.​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..