Skip to main content
Associate
September 5, 2024
Question

Need a level shifter in board MB1441 of STLINK-V3SET debugger

Hi there.

I want to download my bin file to one of my customized board ( target STM32G030F6P6).

The problem is the debugger pin CN1 of Hardware board MB1441 has 5V input but my one has 2.8 V in debug connector.

Kindly recommend a solution for voltage level shifting.

And also share Hardware board MB1441 schematic. 

 

 

BR

HASAN

This topic has been closed for replies.

4 replies

Peter BENSCH
ST Technical Moderator
September 5, 2024

CN1 of the STLINK-V3SET has CMOS 3.3V interfaces, not 5V.

The B-STLINK-VOLT board extension is a 1.65V-3.3V voltage adapter board for the STLINK-V3SET.

The entire toolset is not open source, so the schematics are not publicly available.

Hope that answers your questions?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Hasan2024Author
Associate
September 5, 2024

Peter,

Thank you for clarification.

Do you have CN1 pin map? Let me know. Figure out the location of 1.5 to 3.3v source.

 

Peter BENSCH
ST Technical Moderator
September 5, 2024

You can find the pin map of CN1 in UM2448, section 8.2.1.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.