Skip to main content
JHoev
Visitor II
August 8, 2019
Question

My CubeIDE doesn't find the testboard when I try to debug

Hello

I'm pretty new to the STM32CubeIDE, and try to flash my test-program (a LED-blink programm) on my NUCLEO-F446RE developementboard. If i press the debug-button, the program is compiled, but then i get the folowing Error:

"Error in final launch sequence:

Error in initializing ST-LINK device.

Reason: (4) No device found on target.

Error in initializing ST-LINK device.

Reason: (4) No device found on target."

The frame of the code, i had generated with the HAL-codegenerator.

I have no settings changed in the IDE yet

Now I have no clue what to do, so hopefully somebody here can help me.

Thanks in advance

This topic has been closed for replies.

1 reply

Brian TIDAL
ST Technical Moderator
August 9, 2019

Hi

can you check that the power LED (LD3) is ON (RED LED). If not, can you check that the JP6 (IDD) is properly ON (remove it and put it back) and that JP5(PWR) is in the proper position (U5V).

See https://community.st.com/s/question/0D50X0000B6Q0SMSQ0/stlink-broken-after-upgrade-on-nucleo-card for similar issue.

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.