Skip to main content
Associate III
Jun 4, 2025 8:45 AM UTC
Solved

Measuring power consumption of NUCLEO-N657X0-Q using ST probes

Hi,

 

I'm wondering if there are any recommendations/guidelines when trying to measure power consumption on the Nucleo-N657X0-Q when running a neural network model, both with NPU acceleration and without on the CPU for comparison. I have access to both a X-Nucleo-LPM01A power shield and a STLINK-V3PWR and do not know which one to choose.

 

Are both options rated for enough power to measure the board? And does any of the two options require removing components, as the board is borrowed so I would prefer a non-invasive solution.

 

Thanks in advance!

This topic has been closed for replies.
David SIORPAES
David SIORPAESBest answer
ST Employee
Jun 4, 2025 12:39 PM UTC

Hello,

There is a well documented application that shows how to do power measurements on a DK board.

It should be pretty easy to adapt it to a Nucleo board:

https://github.com/STMicroelectronics/x-cube-n6-ai-power-measurement

It makes use of STLINK-V3PWR but you need hardware modifications though.

 

David

7 replies

David SIORPAES
David SIORPAESBest answer
ST Employee
Jun 4, 2025 12:39 PM UTC

Hello,

There is a well documented application that shows how to do power measurements on a DK board.

It should be pretty easy to adapt it to a Nucleo board:

https://github.com/STMicroelectronics/x-cube-n6-ai-power-measurement

It makes use of STLINK-V3PWR but you need hardware modifications though.

 

David

brianonAuthor
Associate III
Jun 4, 2025 12:57 PM UTC

Hi @David SIORPAES,

 

Do you know if the X-Nucleo-LPM01A approach would also require hardware modifications? If possible I would prefer not to make any hardware modifications as I am still relatively new to working with ST boards.

David SIORPAES
ST Employee
Jun 4, 2025 1:12 PM UTC

Hello,

Being the X-Nucleo-LPM01A a power source too, it would need the same hardware modifications.

The least invasive procedure is to remove R40 and measure the voltage drop on R41 as described here: 

Measuring Current on NUCLEO-N657X0-Q - STMicroelectronics Community

You can then leave R40 unsoldered.

David

 

David SIORPAES
ST Employee
Jun 4, 2025 4:06 PM UTC

The solution with R40 requires to measure the voltage drop using an oscilloscope or other instrument on CN12 3-4 pins. You cannot use a power source such as STLINK-V3PWR to accomplish this.

This solution has the non negligible advantage that the required hardware modifications are less invasive (just remove R40).