Skip to main content
Associate III
Dec 19, 2024 11:34 AM UTC
Solved

Looking for STM32H745II ST board to evaluate ADC

Hi,

I would like to evaluated ADC of STM32H745. I would like to have 12bit 5.12MHz dual ADC. According to my understanding, I need to use model STM32H745II in 176 pin UFBGA to obtain ADC performance. Is there any board like nucleo, which can be used for evaluation?

This topic has been closed for replies.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Dec 19, 2024 12:01 PM UTC

@mosamasa wrote:

According to my understanding, Disco is based on STM32H745XI (240pin TFBGA). Maximum ADC rate would be only 4.38MHz.


Yes you're right according to the AN5354:

SofLit_0-1734618806165.png

But, unfortunately, there is no other ST boards for STM32H745 with other packages.

The only available ST boards for STM32H745 are with LQFP144 and TFBGA240.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

3 replies

mƎALLEm
ST Technical Moderator
Dec 19, 2024 11:44 AM UTC
To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
mosamasaAuthor
Associate III
Dec 19, 2024 11:48 AM UTC

According to my understanding, Disco is based on STM32H745XI (240pin TFBGA). Maximum ADC rate would be only 4.38MHz.

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Dec 19, 2024 12:01 PM UTC

@mosamasa wrote:

According to my understanding, Disco is based on STM32H745XI (240pin TFBGA). Maximum ADC rate would be only 4.38MHz.


Yes you're right according to the AN5354:

SofLit_0-1734618806165.png

But, unfortunately, there is no other ST boards for STM32H745 with other packages.

The only available ST boards for STM32H745 are with LQFP144 and TFBGA240.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.