Skip to main content
SBhuj.1
Associate II
January 18, 2020
Question

Looking for project to build External Loader for STM32F756 for ST Link Utility

We were using Micron NOR flash with STM32F756 as given in EVAL board.

In ST Link we were using option "M29W128GL_STM32F756G-EVAL" for external loader.

Now we have replaced Micron NOR Flash with Cypress NOR Flash.

But above mentioned option is not working for Cypress NOR flash, because Cypress NOR flash timings are different. I need to change in external loader code.

But there is no example project for STM32F756 in its installed path.

Therefore I request this community to give me the code or link for it.

I have one more doubt about ST Link utility.

As per UM0892, after copying ".out" file as ".stldr", will it display in external loader list directly ?

Or

Is there any changes required in ST Link utility GUI, to see that file in External Loader List ?

This topic has been closed for replies.