Skip to main content
flyer31
Senior
May 30, 2021 8:24 AM UTC
Solved

Keil ARMCC V5.1 does not connect to Nucleo 474 (ST-LINK V3)

Is there any way to come around this? Or is this some "dirty trick" of the stupid "STM-Cube-Fan-Group" at STM to force all STM users into their stupid STM-Cube world?

(If I try to connect Keil uVision 5.1 to the new Nucleo ARM G474 boards, the Keil Project properties ST Link Properties page tells me "ST-LINK(too recent)"... with an older V2 STLINK module for G074 Nucleo it will work without problem... I unfortunately really need my old "full Keil license" as in this case I want to try programming some RTOS with more than 32kByte Code - and please do not tell me that I should buy a new Keil ARMCC version only to communicate to this completely unnecessary new STLINK V3 interface, which really nobody needs?)

This topic has been closed for replies.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
May 30, 2021 1:04 PM UTC

The interface code/drivers should reside in the \Keil\ARM\STLink directory.

In times past it was possible to replace or rename DLLs in this directory to support new connectivity/function.

Ping me at sourcer32@gmail.com I'll dig out the working set from here.

Check also the Software directory of the CubeG4 archive, there are sometimes patches there for Keil/IAR tool chains.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

4 replies

flyer31
flyer31Author
Senior
May 30, 2021 11:08 AM UTC

Is there some way on this STLINKV3 interface CPU U5A to somehow "short circuit" the 2 signals STLK_SWDIO, STLK_SWCLK to T_SWDIO, T_SWCLK by some chip signal / solder jumper? ... then I could at list in a nice way come around the STLINK V3 interface and use some other STLINKV2 Nucleo board for access to the STM32G474RE... . I already considered to exchange the 64pin LQFP STM32G470RB chip on my older "good old Nucleo G070RB board" (which has nice ST-LINKV2 interface... . But currently even no chips available ... the distris announce them only for Dec. 2021 / Apr. 2022... this is really tough...).

Super nice would be, if somebody of the so "super-ingenious" ST-LINK V3 group of STM could be motivated to possibly present some update software would would in some way present "backward-compatibility" to ST-LINK V2 software interfaces.. .

flyer31
flyer31Author
Senior
May 30, 2021 11:25 AM UTC

... looking at the schematics, I think the nices way to cut away the disturbing ST-LINK V3 interface on this Nucleo board is to remove JP3, SB40 and SB41, and then connect an external ST-LINK V2 interface to the CN7 Morpho connector at NRST-PA13-PA14 ... just not yet completely sure how to best get the 3V3 from the other STLINK V2 board without shooting the power supplies... .

Any help or helpful comments would be grealy appreciated!

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
May 30, 2021 1:04 PM UTC

The interface code/drivers should reside in the \Keil\ARM\STLink directory.

In times past it was possible to replace or rename DLLs in this directory to support new connectivity/function.

Ping me at sourcer32@gmail.com I'll dig out the working set from here.

Check also the Software directory of the CubeG4 archive, there are sometimes patches there for Keil/IAR tool chains.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
flyer31
flyer31Author
Senior
May 30, 2021 2:37 PM UTC

Wow, you are my hero, thank you very much ... this really helped... I just copied this STLINK subfolder from my Keil (newest version but no licencse) to my old Keil_v5\am of Keil V5.1 ... and now miraculously my good old Keil V5.1 shows "STLINK V3" in the debugger properties debug settings window, and also loading works perfectly... .

This saved me a spoiled day... thank you very much.