Skip to main content
Armin Böss
Associate II
April 3, 2017
Question

Issue with ST Link Update

Posted on April 03, 2017 at 18:14

Hello,

When i connect my STM 32F401RE to the STM32 ST-Link Utility and then try to update the firmware, it says that Version V2.J27.M15 is the latest.

When i do the same with ST-Link Upgrade (stswlink007 from st.com), it says that Version V2.J28.M18 is the latest.

Which Firmware should i install now?

Best Regards

Armin

#st-link #st-link-utility #st-link-update
This topic has been closed for replies.

4 replies

ST Technical Moderator
April 3, 2017
Posted on April 03, 2017 at 18:26

Hi,

I recommend you to upgrade the ST-Link firmware version to V2-1 through this

http://www.st.com/content/st_com/en/products/embedded-software/development-tool-software/stsw-link009.html

Hope this help you.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Tesla DeLorean
Guru
April 4, 2017
Posted on April 04, 2017 at 21:59

>>

Which Firmware should i install now?

Does it matter? Do you have some issue that it might remediate? If it works, just leave it alone.

If you have a problem it makes sense to upgrade before complaining so that past issues aren't continually relitigated, but if things are working there is no need in most cases.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Armin Böss
Associate II
April 4, 2017
Posted on April 04, 2017 at 22:55

Thank yout both for your Quick Answers.

To the Thing with

/external-link.jspa?url=http%3A%2F%2Fwww.st.com%2Fcontent%2Fst_com%2Fen%2Fproducts%2Fembedded-software%2Fdevelopment-tool-software%2Fstsw-linkhtml

: I´ve already installed this and updated it with STSW-LINK007, or is there something about both Software´s i didn´t get?

Yes I have a Issue with my board and i´m currently unsure about wether it´s a software or a hardware issue (my X-Nucleo-53L0A1 shield won´t work most times, just sometimes.....I know it sounds awkward but when i try figuring out whats the problem it feels like someone just rolling the dices about wether my shield will work or not, but i think i´m goint to open a new thread about that Problem tomorrow).

Thank you very much

Tesla DeLorean
Guru
April 5, 2017
Posted on April 05, 2017 at 00:27

They are on different release schedules and software released in the past will not have the most up-to-date firmware.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..