Skip to main content
Visitor II
July 18, 2024
Question

Issue while debugging STM32F410RB

I am used the board for 4hrs single Strech.

Used the proper ST Link debugger.

Console Message:

Target no device found

Error in initializing ST-LINK device.

Reason: No device found on target.

 

This topic has been closed for replies.

2 replies

mƎALLEm
ST Technical Moderator
July 18, 2024

Hello @unknownVSS  and welcome to the community,

You didn't mention which board you are using? is it NUCLEO-F410RB?

You need first to check your USB cable. You need to use a data cable instead of charging cable.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
TDK
July 18, 2024

Also note that if you don't properly close a debugging session, the st-link is still in use. The st-link communication LED should indicate if this is the case. Power cycling the board and/or rebooting computer will likely clear up any remaining issues.

"If you feel a post has answered your question, please click ""Accept as Solution""."