Skip to main content
Associate
August 26, 2025
Question

Issue Activating Peripherals with STM32h745i Disco board

Hi Fellow Developers,

There is actually some issue while trying to configure the peripherals on the disco board.

Be it USART or SPI even after selecting the core for a particular communication protocol on board i am unable to get an response over it. Earlier i was trying to configure SPI and read a external SD CARD over SPI but am unable to get an response over SPI. 

I even checked pins over oscilloscope and had not clock or data over MISO or MOSI.
As mentioned at below pins.

mehrotraAkshay_0-1755858593376.png


Then i tried sending data over USART3 pins and had no response there either.

mehrotraAkshay_2-1755858972367.jpeg

Green is Tx connected to Pin D0 which is Rx on STM board
Blue is Rx connected to Pin D1 which is Tx on STM board
And Orange is GND.
I know HW connections are right, provided for reference.

Also here is a basic code of USART transmit.

int main(void)
{

 /* USER CODE BEGIN 1 */
	uint8_t txData[] ="Hello M7-DISCO!\r\n";

 /* USER CODE END 1 */
/* USER CODE BEGIN Boot_Mode_Sequence_0 */
#if defined(DUAL_CORE_BOOT_SYNC_SEQUENCE)
 int32_t timeout;
#endif /* DUAL_CORE_BOOT_SYNC_SEQUENCE */
/* USER CODE END Boot_Mode_Sequence_0 */

/* USER CODE BEGIN Boot_Mode_Sequence_1 */
#if defined(DUAL_CORE_BOOT_SYNC_SEQUENCE)
 /* Wait until CPU2 boots and enters in stop mode or timeout*/
 timeout = 0xFFFF;
 while((__HAL_RCC_GET_FLAG(RCC_FLAG_D2CKRDY) != RESET) && (timeout-- > 0));
 if ( timeout < 0 )
 {
 Error_Handler();
 }
#endif /* DUAL_CORE_BOOT_SYNC_SEQUENCE */
/* USER CODE END Boot_Mode_Sequence_1 */
 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();
/* USER CODE BEGIN Boot_Mode_Sequence_2 */
#if defined(DUAL_CORE_BOOT_SYNC_SEQUENCE)
/* When system initialization is finished, Cortex-M7 will release Cortex-M4 by means of
HSEM notification */
/*HW semaphore Clock enable*/
__HAL_RCC_HSEM_CLK_ENABLE();
/*Take HSEM */
HAL_HSEM_FastTake(HSEM_ID_0);
/*Release HSEM in order to notify the CPU2(CM4)*/
HAL_HSEM_Release(HSEM_ID_0,0);
/* wait until CPU2 wakes up from stop mode */
timeout = 0xFFFF;
while((__HAL_RCC_GET_FLAG(RCC_FLAG_D2CKRDY) == RESET) && (timeout-- > 0));
if ( timeout < 0 )
{
Error_Handler();
}
#endif /* DUAL_CORE_BOOT_SYNC_SEQUENCE */
/* USER CODE END Boot_Mode_Sequence_2 */

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_USART2_UART_Init();
 /* USER CODE BEGIN 2 */

 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
	 HAL_UART_Transmit(&huart2, txData, sizeof(txData), HAL_MAX_DELAY);
	 		 HAL_Delay(1000);
 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}


I tried for both cores simultaneously M7 and M4. But received no response.

Is there a specific configuration which needs to be done to initiate the pins as required peripherals which i am missing?



 

This topic has been closed for replies.

2 replies

mƎALLEm
ST Technical Moderator
August 26, 2025

Hello,

Not clear what the problem is and I don't see any code related to SPI. Are you testing in debug mode? if yes that's tricky in Dual core. Are you really using both cores at the same time in your example?

Start by toggling a LED first then move on to SPI/UART communication.

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Associate
August 27, 2025

Hi,
Thanks for Replying.
Yes I am testing debug mode, and yes i am using both cores in my example. Earlier I had toggled LED 1 on M7 core and LED 2 on M4 core in parallel and it was working.

Issue us that i am getting no response on UART or SPI pin of ARDUINO connectors given on board.
Mentioned below for your reference.

mehrotraAkshay_0-1756289123477.png

And below is the normal SPI data send code - (tried with and without DMA both) along with configuration, also attaching complete example project for further reference. On checking clock via oscilloscope there is no waveform on board pin D13 or MCU pin PD3.

//main.c

/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{
 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */
/* USER CODE BEGIN Boot_Mode_Sequence_0 */
 int32_t timeout;
/* USER CODE END Boot_Mode_Sequence_0 */

/* USER CODE BEGIN Boot_Mode_Sequence_1 */
 /* Wait until CPU2 boots and enters in stop mode or timeout*/
 timeout = 0xFFFF;
 while((__HAL_RCC_GET_FLAG(RCC_FLAG_D2CKRDY) != RESET) && (timeout-- > 0));
 if ( timeout < 0 )
 {
 Error_Handler();
 }
/* USER CODE END Boot_Mode_Sequence_1 */
 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();
/* USER CODE BEGIN Boot_Mode_Sequence_2 */
/* When system initialization is finished, Cortex-M7 will release Cortex-M4 by means of
HSEM notification */
/*HW semaphore Clock enable*/
__HAL_RCC_HSEM_CLK_ENABLE();
/*Take HSEM */
HAL_HSEM_FastTake(HSEM_ID_0);
/*Release HSEM in order to notify the CPU2(CM4)*/
HAL_HSEM_Release(HSEM_ID_0,0);
/* wait until CPU2 wakes up from stop mode */
timeout = 0xFFFF;
while((__HAL_RCC_GET_FLAG(RCC_FLAG_D2CKRDY) == RESET) && (timeout-- > 0));
if ( timeout < 0 )
{
	Error_Handler();
}
/* USER CODE END Boot_Mode_Sequence_2 */

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
#if(UART_ENABLE)
 MX_DMA_Init();
 MX_USART3_UART_Init();
#endif
 MX_SPI2_Init();
 Spi_state = TRANSFER_WAIT;
#ifdef MASTER_BOARD
	while (HAL_GPIO_ReadPin(B1_GPIO_Port,B1_Pin) != GPIO_PIN_SET)
	{
		HAL_Delay(100);
	}
#endif
 /* USER CODE BEGIN 2 */
 /*##-2- Start the Full Duplex Communication process ########################*/
 /* While the SPI in TransmitReceive process, user can transmit data through
 "aTxBuffer" buffer & receive data through "aRxBuffer" */
 if(HAL_SPI_TransmitReceive_DMA(&hspi2, (uint8_t*)aTxBuffer, (uint8_t *)aRxBuffer, BUFFERSIZE) != HAL_OK)
 {
 /* Transfer error in transmission process */
 Error_Handler();
 }
#if(UART_ENABLE)
 HAL_UART_Transmit(&huart3,(unsigned char*)aRxBuffer,strlen(aRxBuffer),10);
 HAL_Delay(10);
#endif
 /*##-3- Wait for the end of the transfer ###################################*/
 /* Before starting a new communication transfer, you must wait the callback call
 to get the transfer complete confirmation or an error detection.
 For simplicity reasons, this example is just waiting till the end of the
 transfer, but application may perform other tasks while transfer operation
 is ongoing. */
 while (Spi_state == TRANSFER_WAIT)
 {
#if(UART_ENABLE)
 HAL_UART_Transmit(&huart3,(unsigned char*)"waiting\n\r",strlen("waiting\n\r"),10);
 HAL_Delay(2);
#endif
 }

 switch(Spi_state)
 {
 case TRANSFER_COMPLETE :
 /*##-4- Compare the sent and received buffers ##############################*/
#if(UART_ENABLE)
 	HAL_UART_Transmit(&huart3,(unsigned char*)aRxBuffer,strlen(aRxBuffer),10);
 	HAL_Delay(10);
#endif
 if(Buffercmp((uint8_t*)aTxBuffer, (uint8_t*)aRxBuffer, BUFFERSIZE))
 {
 /* Processing Error */
 Error_Handler();
 }
 break;
 default :
 Error_Handler();
 break;
 }
 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}

/**
 * @brief SPI2 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_SPI2_Init(void)
{

 /* USER CODE BEGIN SPI2_Init 0 */

 /* USER CODE END SPI2_Init 0 */

 /* USER CODE BEGIN SPI2_Init 1 */

 /* USER CODE END SPI2_Init 1 */
 /* SPI2 parameter configuration*/
 hspi2.Instance = SPI2;
 hspi2.Init.Mode = SPI_MODE_MASTER;
 hspi2.Init.Direction = SPI_DIRECTION_2LINES;
 hspi2.Init.DataSize = SPI_DATASIZE_4BIT;
 hspi2.Init.CLKPolarity = SPI_POLARITY_LOW;
 hspi2.Init.CLKPhase = SPI_PHASE_1EDGE;
 hspi2.Init.NSS = SPI_NSS_SOFT;
 hspi2.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_2;
 hspi2.Init.FirstBit = SPI_FIRSTBIT_MSB;
 hspi2.Init.TIMode = SPI_TIMODE_DISABLE;
 hspi2.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
 hspi2.Init.CRCPolynomial = 0x0;
 hspi2.Init.NSSPMode = SPI_NSS_PULSE_ENABLE;
 hspi2.Init.NSSPolarity = SPI_NSS_POLARITY_LOW;
 hspi2.Init.FifoThreshold = SPI_FIFO_THRESHOLD_01DATA;
 hspi2.Init.TxCRCInitializationPattern = SPI_CRC_INITIALIZATION_ALL_ZERO_PATTERN;
 hspi2.Init.RxCRCInitializationPattern = SPI_CRC_INITIALIZATION_ALL_ZERO_PATTERN;
 hspi2.Init.MasterSSIdleness = SPI_MASTER_SS_IDLENESS_00CYCLE;
 hspi2.Init.MasterInterDataIdleness = SPI_MASTER_INTERDATA_IDLENESS_00CYCLE;
 hspi2.Init.MasterReceiverAutoSusp = SPI_MASTER_RX_AUTOSUSP_DISABLE;
 hspi2.Init.MasterKeepIOState = SPI_MASTER_KEEP_IO_STATE_DISABLE;
 hspi2.Init.IOSwap = SPI_IO_SWAP_DISABLE;
 if (HAL_SPI_Init(&hspi2) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN SPI2_Init 2 */

 /* USER CODE END SPI2_Init 2 */

}

// in msp.c
/**
 * @brief SPI MSP Initialization
 * This function configures the hardware resources used in this example
 * @PAram hspi: SPI handle pointer
 * @retval None
 */
void HAL_SPI_MspInit(SPI_HandleTypeDef* hspi)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
 RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
 if(hspi->Instance==SPI2)
 {
 /* USER CODE BEGIN SPI2_MspInit 0 */

 /* USER CODE END SPI2_MspInit 0 */

 /** Initializes the peripherals clock
 */
 PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_SPI2;
 PeriphClkInitStruct.Spi123ClockSelection = RCC_SPI123CLKSOURCE_PLL;
 if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /* Peripheral clock enable */
 __HAL_RCC_SPI2_CLK_ENABLE();

 __HAL_RCC_GPIOD_CLK_ENABLE();
 __HAL_RCC_GPIOI_CLK_ENABLE();
 __HAL_RCC_GPIOB_CLK_ENABLE();
 /**SPI2 GPIO Configuration
 PD3 ------> SPI2_SCK
 PI2 ------> SPI2_MISO
 PB15 ------> SPI2_MOSI
 */
 GPIO_InitStruct.Pin = GPIO_PIN_3;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 GPIO_InitStruct.Alternate = GPIO_AF5_SPI2;
 HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);

 GPIO_InitStruct.Pin = GPIO_PIN_2;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 GPIO_InitStruct.Alternate = GPIO_AF5_SPI2;
 HAL_GPIO_Init(GPIOI, &GPIO_InitStruct);

 GPIO_InitStruct.Pin = GPIO_PIN_15;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 GPIO_InitStruct.Alternate = GPIO_AF5_SPI2;
 HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

 /* SPI2 DMA Init */
 /* SPI2_RX Init */
 hdma_spi2_rx.Instance = DMA1_Stream0;
 hdma_spi2_rx.Init.Request = DMA_REQUEST_SPI2_RX;
 hdma_spi2_rx.Init.Direction = DMA_PERIPH_TO_MEMORY;
 hdma_spi2_rx.Init.PeriphInc = DMA_PINC_DISABLE;
 hdma_spi2_rx.Init.MemInc = DMA_MINC_ENABLE;
 hdma_spi2_rx.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;
 hdma_spi2_rx.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;
 hdma_spi2_rx.Init.Mode = DMA_NORMAL;
 hdma_spi2_rx.Init.Priority = DMA_PRIORITY_LOW;
 hdma_spi2_rx.Init.FIFOMode = DMA_FIFOMODE_DISABLE;
 if (HAL_DMA_Init(&hdma_spi2_rx) != HAL_OK)
 {
 Error_Handler();
 }

 __HAL_LINKDMA(hspi,hdmarx,hdma_spi2_rx);

 /* SPI2_TX Init */
 hdma_spi2_tx.Instance = DMA1_Stream1;
 hdma_spi2_tx.Init.Request = DMA_REQUEST_SPI2_TX;
 hdma_spi2_tx.Init.Direction = DMA_MEMORY_TO_PERIPH;
 hdma_spi2_tx.Init.PeriphInc = DMA_PINC_DISABLE;
 hdma_spi2_tx.Init.MemInc = DMA_MINC_ENABLE;
 hdma_spi2_tx.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;
 hdma_spi2_tx.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;
 hdma_spi2_tx.Init.Mode = DMA_NORMAL;
 hdma_spi2_tx.Init.Priority = DMA_PRIORITY_LOW;
 hdma_spi2_tx.Init.FIFOMode = DMA_FIFOMODE_DISABLE;
 if (HAL_DMA_Init(&hdma_spi2_tx) != HAL_OK)
 {
 Error_Handler();
 }

 __HAL_LINKDMA(hspi,hdmatx,hdma_spi2_tx);

 /* SPI2 interrupt Init */
 HAL_NVIC_SetPriority(SPI2_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(SPI2_IRQn);
 /* USER CODE BEGIN SPI2_MspInit 1 */

 /* USER CODE END SPI2_MspInit 1 */

 }

}

/**
 * @brief SPI MSP De-Initialization
 * This function freeze the hardware resources used in this example
 * @PAram hspi: SPI handle pointer
 * @retval None
 */
void HAL_SPI_MspDeInit(SPI_HandleTypeDef* hspi)
{
 if(hspi->Instance==SPI2)
 {
 /* USER CODE BEGIN SPI2_MspDeInit 0 */

 /* USER CODE END SPI2_MspDeInit 0 */
 /* Peripheral clock disable */
 __HAL_RCC_SPI2_CLK_DISABLE();

 /**SPI2 GPIO Configuration
 PD3 ------> SPI2_SCK
 PI2 ------> SPI2_MISO
 PB15 ------> SPI2_MOSI
 */
 HAL_GPIO_DeInit(GPIOD, GPIO_PIN_3);

 HAL_GPIO_DeInit(GPIOI, GPIO_PIN_2);

 HAL_GPIO_DeInit(GPIOB, GPIO_PIN_15);

 /* SPI2 DMA DeInit */
 HAL_DMA_DeInit(hspi->hdmarx);
 HAL_DMA_DeInit(hspi->hdmatx);

 /* SPI2 interrupt DeInit */
 HAL_NVIC_DisableIRQ(SPI2_IRQn);
 /* USER CODE BEGIN SPI2_MspDeInit 1 */

 /* USER CODE END SPI2_MspDeInit 1 */
 }

}