Skip to main content
RSmal.2
Associate II
February 9, 2022
Solved

Is it possible to use ST-LINK V2 to program/debug a NUCLEO-F401RE board using STM32CUBEIDE. I receive "Error Initializing ST-LINK device. No target found" I can explain more if needed.

..

This topic has been closed for replies.
RSmal.2
RSmal.2Best answer
Associate II
February 9, 2022

I figured it out. I was unaware that NRST needed to be wired as well. This fixed the issue.

6 replies

SSmit.12
Visitor II
February 9, 2022

Yes it can be possible

RSmal.2
RSmal.2Author
Associate II
February 9, 2022

Would you be able to elaborate? I have the VDD, GND, SWCLK, and SWDIO pins from the ST-LINK to the nucleo board using the ST MORPHO CN7. I installed the driver for ST-LINK V2 (STSW-LINK009), but I continue to get an No target device found error when debugging. I also removed the jumpers on CN2

RSmal.2
RSmal.2Author
Associate II
February 9, 2022

Would you be able to elaborate? I have the VDD, GND, SWCLK, and SWDIO pins from the ST-LINK to the nucleo board using the ST MORPHO CN7. I installed the driver for ST-LINK V2 (STSW-LINK009), but I continue to get an No target device found error when debugging. I also removed the jumpers on CN2

TDK
February 9, 2022

The nucleo board has a built-in programmer. Is there a reason you're not just using that?

You can program it externally, but you need to ensure the onboard programmer is disconnected.

Is the board powered?

Can STM32CubeProgrammer connect? What target voltage does it detect?

"If you feel a post has answered your question, please click ""Accept as Solution""."
RSmal.2
RSmal.2Author
Associate II
February 9, 2022

The nucleo board works with no problems with the built in programmer. I am not using that because I will be using ST-LINK to debug/program using SWD on a custom board so I would like to see what it takes. The board is power using the USB connector on the board. I am using STM32CUBEIDE and it sees the ST-LINK and the target voltage is 3.3V. Do you have additional info on how to ensure the onboard programmer is disconnected? The USB i am using to power the board is not connected to my computer.

RSmal.2
RSmal.2AuthorBest answer
Associate II
February 9, 2022

I figured it out. I was unaware that NRST needed to be wired as well. This fixed the issue.