Skip to main content
Lead
February 8, 2020
Question

Is it possible to program the Chinese clone "Blue Pill" with a Nucleo board?

Hi!

I did buy a Chinese clone "Blue Pill" that are supposed to work as a real STM32. When I looked at the chip, it was not a STM32 chip. It was a CS32F103C8T6 chip instead of STM32F103C8T6

Now I'm have connecting the ST-link from my Nucleo board to the Blue Pill, and the ST-link cannot recognize the Blue Pill board.

Vendor = 0x3B
 
Error in initializing ST-LINK device.
Reason: ST-LINK: Could not verify ST device! Abort connection.

Does that mean that it's NOT possible to program these Chinese clones with ST-Link and CubeMX, or is there a walk around?

I can see that lots of people have the same issue.

https://forum.atollic.com/viewtopic.php?t=1651

Link to the Blue Pill

https://www.banggood.com/STM32F103C8T6-Small-System-Development-Board-Microcontroller-STM32-ARM-Core-Board-p-1058299.html?rmmds=myorder

This topic has been closed for replies.

1 reply

KnarfB
Super User
February 9, 2020

You should better ask the chinese clone forum.