Skip to main content
Associate III
April 13, 2024
Solved

Is it OK to Solder 0.1 inch connector pins on ST-LinkV3MiniE PCB edge connector?

V3MiniE is 2mm pitch, total 10mm at outer most gold finger pcb trace.   Two rows of  5 pins 2.54mm pins is 10.16mm at centre, for top an dbottom gold finger.  It will work ok, right?  TIA

 

David__0-1713050536823.png

 

 

This topic has been closed for replies.
AScha.3
AScha.3Best answer
Super User
April 14, 2024

Sure, if you center the "wrong" as good as possible and can solder, without making a short to next pin.

Especially the 1. and 5. are no more on the copper trace, but only thick solder joint can bridge the gap here;

but if you  can do this - its ok.

It could look like mine here :  :)

AScha3_0-1713079733155.png

 

If you feel a post has answered your question, please click on " Best Answer ".

2 replies

AScha.3
AScha.3Best answer
Super User
April 14, 2024

Sure, if you center the "wrong" as good as possible and can solder, without making a short to next pin.

Especially the 1. and 5. are no more on the copper trace, but only thick solder joint can bridge the gap here;

but if you  can do this - its ok.

It could look like mine here :  :)

AScha3_0-1713079733155.png

 

If you feel a post has answered your question, please click on " Best Answer ".
David_Author
Associate III
April 14, 2024

Many thanks