Interrupts are not triggered during firmware-in-SRAM debugging using ST-Link
- 2 replies
- 1364 views
Hi,
I have implemented my application firmware on STM32F746G discovery board and it worked fine while the code was located in embedded flash (just like most examples in cube).
Now I am trying to migrate code to SRAM using ST-Link, to evaluate the execution time between code in flash and RAM.
Current status is that the break points in main() could be reached, but the program was stalled in HAL_Delay() since the interrupt SysTick_Handler() was never triggered. I've spent all day long without finding any useful hint...
My environment is Keil uVision 5, and here is what I did to configure ST-Link debugging in SRAM:
- Change memory areas in Target tab IROM1: 0x20000000, 0x10000 IRAM1: 0x20010000, 0x40000
- Add a define in C/C++ tab: VECT_TAB_SRAM
- Add debug init file (RAM.ini) and uncheck 'Load Application at Startup' in Debug tab
FUNC void Setup (void) {
SP = _RDWORD(0x20000000); // Setup Stack Pointer PC = _RDWORD(0x20000004); // Setup Program Counter XPSR = 0x01000000; // Set Thumb Bit _WDWORD(0xE000ED08, 0x20000000); // Setup Vector Table Offset Register}LOAD %L INCREMENTAL // Download to RAM
Setup();// g, main
- Uncheck 'Update Target before Debugging' in Utilities tab
- Press Settings button in Utilities tab, In Flash Download tab1. Download function: Do not erase2. RAM for Algorithm: 0x20010000, 0x10003. Programming Algorithm: 20000000H - 2000FFFFH
Enclosed is a sample to describe my problem. Note that it's based on cube so it should be placed into the cube directory.
Thanks in advance.
#debug #stm32f7-discovery #st-link