Skip to main content
Associate III
September 1, 2024
Question

Internal ADC

  • I'm using nucleo f446 board for adc sampling the internal adc is unidirectional. 
  • Is there any other development board like nucleo or discovery with internal ADC which can give both positive and negative cycle of adc
  • Please suggest me so that I can avoid external adc.
This topic has been closed for replies.

4 replies

KnarfB
Super User
September 1, 2024

>  internal ADC which can give both positive and negative cycle of adc

do you mean differential input channels?

Check out the STM32G4 series, like NUCLEO-G474RE

hth

KnarfB

TDK
September 3, 2024

No STM32 chips can convert a negative voltage. The voltage range is always limited from 0 V to VREF+, even in differential mode. External ADCs will have the same limitation.

"If you feel a post has answered your question, please click ""Accept as Solution""."
harry123Author
Associate III
September 3, 2024
  • I want to read both positive and negative cycle of a sine wave.
  • Whenever I start adc sampling only positive values are given all negative values will be zero 
  • Is there any solution 

Thank you 

TDK
September 3, 2024

The STM32 cannot convert negative voltages. Nothing can change that.

Create external circuitry to change the input to be always positive. AC coupling could be a possibility.

"If you feel a post has answered your question, please click ""Accept as Solution""."