Skip to main content
This topic has been closed for replies.

4 replies

Peter BENSCH
ST Technical Moderator
September 12, 2024

Welcome @JanhaviDeshpande, to the community!

Many details are still missing:

  • buzzer data sheet (link to the data sheet would be fine)
  • what supply voltage will the buzzer have
  • what frequencies should the buzzer emit and at what volume?
  • which waveforms should be sent to the buzzer?
  • are you planning to use an amplifier stage, if so, which one (or do you need proposals)?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
JanhaviDeshpande
Associate
September 12, 2024

First of all, Thankyou Sir for replying to the message.

Basically, using TMB12A05 active buzzer for a project based on anamoly detection based on audio. Basic functioning includes giving alert. 

Karl Yamashita
Principal
September 12, 2024

@JanhaviDeshpande wrote:

First of all, Thankyou Sir for replying to the message.

Basically, using TMB12A05 active buzzer for a project based on anamoly detection based on audio. Basic functioning includes giving alert. 


Still not enough information on what you're trying to achieve.

  • "based on audio" - So do you have something that detects this audio? Microphone? Describe what this anomaly consists of.
  • The buzzer has a frequency range of 2300+/-300H. You need to have some kind of driver for it as well, which you haven't provided any schematic.
If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source