Skip to main content
Visitor II
Jul 14, 2025 12:04 PM UTC
Solved

interface a camera with STM32F469I-DISC0 when not all DCMI data pins exposed?

Hi everyone,

I'm trying to interface a DVP camera (like OV5640) with the STM32F469I-DISC0 board using the DCMI peripheral in 8-bit parallel mode.

What I have:
- The camera is configured and outputs data correctly via I2C.
- I'm using bare-metal code (no HAL or CubeMX), and SDRAM + USART debug are working.
- DCMI pins are being mapped as per the STM32F469 reference manual.
- I verified that I can access and remap the following DCMI pins:
- D0 – available
- D1 – available
- D2 – available
- D3 – available
- D4 – not available(e.g., PE5)
- D5 – available 
- D6 – available
- D7 – available
- HSYNC, VSYNC, PCLK – available

Problem:
- DCMI_D4 is not brought out on any connector** on the DISC0 board. It's internally routed to LCD or unused.
- I checked the board schematic and there’s no easy way to solder to it either.

My questions:
1. Can DCMI work with 7-bit data (skipping D4)? Will DCMI capture still be valid if D4 always reads 0?
2. Is there any known workaround for the missing D4 line (e.g., using a dummy input, or masking D4 at software level)?
3. Has anyone successfully interfaced a camera with this DISC0 board and ignored one DCMI data line?
4. Would you recommend switching to 4-bit mode or dropping down to RGB444 or YUV422 and masking bits?

Additional context:
- My goal is to capture camera frames in RGB565 or YUV format and display/stream/debug from SDRAM.
- I’m okay to accept reduced image quality if 1 bit is lost (e.g., D4 = 0 always), but want to understand if DCMI handles this gracefully or fails.

Thanks in advance for any insights or prior experiences!

Sanjay S K

KDJEM.1
KDJEM.1Best answer
ST Technical Moderator
Aug 22, 2025 9:09 AM UTC

Hello @sanjaykrishnegowda and welcome to the community;

 

According to reference manual the DCMI main features are:
• 8-, 10-, 12- or 14-bit parallel interface
• Embedded/external line and frame synchronization
• Continuous or snapshot mode
• Crop feature
• Supports the following data formats:
– 8/10/12/14-bit progressive video: either monochrome or raw Bayer
– YCbCr 4:2:2 progressive video
– RGB 565 progressive video
– Compressed data: JPEG

KDJEM1_0-1755851777300.png

7 bits mode is not supported.

KDJEM1_1-1755853617145.png

Note that the DCMI_D4 is available on PE4, PC11 and PH14 pins.

 

Thanks and best regards,

Kaouthar

 

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.

2 replies

KDJEM.1
KDJEM.1Best answer
ST Technical Moderator
Aug 22, 2025 9:09 AM UTC

Hello @sanjaykrishnegowda and welcome to the community;

 

According to reference manual the DCMI main features are:
• 8-, 10-, 12- or 14-bit parallel interface
• Embedded/external line and frame synchronization
• Continuous or snapshot mode
• Crop feature
• Supports the following data formats:
– 8/10/12/14-bit progressive video: either monochrome or raw Bayer
– YCbCr 4:2:2 progressive video
– RGB 565 progressive video
– Compressed data: JPEG

KDJEM1_0-1755851777300.png

7 bits mode is not supported.

KDJEM1_1-1755853617145.png

Note that the DCMI_D4 is available on PE4, PC11 and PH14 pins.

 

Thanks and best regards,

Kaouthar

 

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.
Visitor II
Feb 19, 2026 9:04 PM UTC

Edit : I soldered the SDCard pin and have been using that for DCMI . Looks like that is the only way.