Skip to main content
Jim Frederick
Associate II
November 20, 2015
Question

Implementing a 'live watch' window in C# test app using ST-Link

Posted on November 20, 2015 at 20:12

I'd like to implement something like IAR's EWARM 'live-watch' window in a C♯ app on a PC to interrogate firmware values via an ST-Link. I'd use this for production testing or diagnostics. The 'live watch' window in EWARM will read parameters over an ST-Link without pausing execution of firmware. It also allows writing too.

In lieu of this, we use a UART or CAN bus but it would be nice to eliminate redundant hardware connections and use the ST-Link since it's needed for initial programming anyway.

Does anybody do this? Is there an API or DLL available to implement this type of communications?

-Jim

#api #st-link-c
This topic has been closed for replies.

4 replies

Tesla DeLorean
Guru
November 22, 2015
Posted on November 22, 2015 at 01:45

http://www.st.com/web/en/catalog/tools/FM146/CL1984/SC720/SS1450/PF210568?sc=stvp

And of course Segger makes a business out of JTAG and programming automation, with DLL/LIB support.

Test points for JTAG and USART connectivity aren't hugely burdensome.

 

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
LaurentL
ST Employee
November 23, 2015
Posted on November 23, 2015 at 16:52

Hello,

Maybe have a look at STM Studio software :

http://www.st.com/web/catalog/tools/FM147/CL1794/SC961/SS1533/PF251373

There is no dll or api you can use with this soft but it can be used to diagnose/test your appli without modifying your appli code.

Rgds,

Laurent
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
jamie2
Associate
March 21, 2016
Posted on March 21, 2016 at 14:16

The SOMNIUM DRT Cortex-M IDE also supports live viewing of variables / expressions while debugging:

http://somniumtech.com/software-tools/somnium-drt-cortex-m-ide
Tesla DeLorean
Guru
March 21, 2016
Posted on March 21, 2016 at 16:53

''Our team's 100+ man years' experience combines business development, operations, microprocessor design and software engineering leadership roles at start-ups through to major international companies.''

So is that like 3 guys with 33+ years in the industry? Your copy editor must have thought that sounded good, it just has me scratching my head.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..