Skip to main content
ZExpo.1
Associate III
Sep 17, 2023 9:04 AM UTC
Solved

I2C Data Transfer Problem

I am trying to send data over I2C3 Using STM32F429 Dev Board and Everyting works fine except the HEX Data I want to send

I am Passing this function

 

HAL_I2C_Mem_Write(&hi2c3,0x30<<1,0x09,I2C_MEMADD_SIZE_8BIT,0XFF,1,100);

 

And Getting the Following Output on Logic Analyzer

 

write to 0x30 ack data: 0x09 0x08 

 

Why I am getting 0x08 instead of 0xFF?

 

 

This topic has been closed for replies.
AScha.3
AScha.3Best answer
Super User
Sep 17, 2023 9:40 AM UTC

right. parameter "0XFF" wrong, needs to be a pointer to the data.

If you feel a post has answered your question, please click on " Best Answer ".

2 replies

waclawek.jan
Super User
Sep 17, 2023 9:18 AM UTC

I don't use Cube/HAL, but you are probably supposed to pass a pointer to an array of bytes, rather than individual values.

JW

AScha.3
AScha.3Best answer
Super User
Sep 17, 2023 9:40 AM UTC

right. parameter "0XFF" wrong, needs to be a pointer to the data.

If you feel a post has answered your question, please click on " Best Answer ".