Skip to main content
JMene.1
Associate II
May 16, 2023
Question

I use the Nucleo-L152 and if I remove the jumper 6 and jumper 5, I get a voltage between +3V3 and VDD of 2.5V and a current of 750uA. Can you explain where this voltage and current are coming from?

..

This topic has been closed for replies.

1 reply

KnarfB
Super User
May 16, 2023

There are signal pins (SWD, UART) from ST-LINK MCU to the L152RE which will "power" the L152RE when Vdd is not connected (J5 open). The GPIO protection diodes are then in the forward direction, which also explains the voltage drop of ~0.7V

hth

KnarfB