Skip to main content
Associate II
October 30, 2023
Solved

I just received the STM32F429I-DISC1 but there is no usb cable, is that normal?

As the title says I just got the stm32f429I-disc1, I was really excited but I realized I couldn't start to play with it because there is no usb cable to connect a PC to the board.

Is it normal?

This topic has been closed for replies.
Imen.DBest answer
ST Technical Moderator
November 1, 2023

Hi @KarlY,

Let me first welcome you to the Community :)

Additional hardware accessories are needed to use the board and run your applications:
– ‘USB type A to Micro-B' cable, used to connect the board (through USB connector CN5) as USB Device to host PC.

I invite you to check the hardware environments and development recommendations required to build your application around the STM32F429-Disco through this UM1662 Getting started with the STM32F429 Discovery kit.

If you still have issues, don't hesitate to come back to the Community either with new threads or as a continuity of this one (when related to same initial topic).

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks

4 replies

Tesla DeLorean
Guru
October 30, 2023

Yes, None of the NUCLEO or DISCO boards come with cables.

You'll need a Mini-USB data cable

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
KarlYAuthor
Associate II
October 31, 2023

Oh okay.. does STMicroelectronics sell cable? Also which type do I need to buy ?

Tesla DeLorean
Guru
November 1, 2023

ST isn't in that business, it's a standard Mini-B cable sort of thing you might have lying around or grab from Amazon. Bit chunkier than the Micro-B used for charging these days, but the connector is more robust and less likely to tear off at the first opportunity. 

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Imen.DBest answer
ST Technical Moderator
November 1, 2023

Hi @KarlY,

Let me first welcome you to the Community :)

Additional hardware accessories are needed to use the board and run your applications:
– ‘USB type A to Micro-B' cable, used to connect the board (through USB connector CN5) as USB Device to host PC.

I invite you to check the hardware environments and development recommendations required to build your application around the STM32F429-Disco through this UM1662 Getting started with the STM32F429 Discovery kit.

If you still have issues, don't hesitate to come back to the Community either with new threads or as a continuity of this one (when related to same initial topic).

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks