Skip to main content
Hawkeye
Associate II
February 16, 2022
Question

I cant get the STlink to work with the programmer. The programmer just closes itself. I have it on the drone01 development board.

  • February 16, 2022
  • 6 replies
  • 1558 views

..

This topic has been closed for replies.

6 replies

Tesla DeLorean
Guru
February 16, 2022

Sorry to hear that, is this a problem you're looking to share or solve?

What OS?

What JRE?

What version of ST-LINK, with what version of firmware?

Did it ever work?

File paths pointing to network drives you're no longer connected too?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Hawkeye
HawkeyeAuthor
Associate II
February 17, 2022

I finally figured it out but was running Linux mint 19.3 and latest version of st-stlink

TDK
February 17, 2022

> drone01 development board

This board does not appear to have an on-board programmer. Are you using an external one? Which one and how is it connected?

Does STM32CubeProgrammer open without anything connected?

"If you feel a post has answered your question, please click ""Accept as Solution""."
Hawkeye
HawkeyeAuthor
Associate II
February 17, 2022

Im using the stm32 programmer with stlink and yes it will open without anything connected to it. I finally figured it out​, had to do with the drone board. Thanks for the quick response

David Littell
Senior II
February 17, 2022

I see this with a V2 up-to-date-with Programmer 2.9 under Ubuntu 18.04 LTS when the target processor (H7B3 in this case) can't immediately be grabbed by the ST-LINK. Click "Connect" and Programmer just crashes. It didn't used to work this way with older Programmer versions but ST helpfully inserted this bug in their never-ending rush to add features at the cost of reliability and robustness.

Hawkeye
HawkeyeAuthor
Associate II
February 17, 2022
I finally have it going. It was the way the drone 1 board was designed. I had to have the USB, the stlink and an ext power supply or battery connected.
Sent from my Galaxy