Skip to main content
Asoni.1
Associate II
July 13, 2020
Question

I am using Nucleo-g431rb, I want to program and debug it with isolation from computer, I am trying to use st-link/V2 isol, but no success, because I can't find the connector for CN10. What is the way to debug it with isolation.

..

This topic has been closed for replies.

2 replies

July 13, 2020

Hello,

Since the nucleo already has the debuger embedded, I suggest using a USB isolator between the PC and the nucleo.

Something like Adafruit USB isolator, which works fine as long as your device does not need more than 100mA.

Asoni.1
Asoni.1Author
Associate II
July 13, 2020

@Kraal​ Yes I am looking for that option also, but it would be an advantage to know if there is anything like st-link available for this type of board.