On the MicroPython website you will find a bunch of different boards and prepared binaries, also created for NUCLEO boards. Some of the targets don't provide USB, like your STM32L031, so maybe you could copy some parts of the schematics from the NUCLEO_F091RC or the NUCLEO_F401RE. Both are based on the same board MB1136, which also contains the debugger ST-LINK/V2-1, but in your design you can connect an ST-LINK externally using SWD pins of your STM32L031F4P3 (pin 19, 20).
Alternatively, you can also use UART2 or SPI1 for programming, but this would require an UART or an SPI interface and some user interaction, since BOOT0=1 and nBOOT1=1 must be set for the internal bootloader (see AN2606, pattern 2).
Regards,
/Peter
In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.