Skip to main content
DHRyu
Associate
April 10, 2023
Question

I am going to design a schematic with STM32H723. I need the STM32h723 reference schematic for the eMMC. There is no eMMC schematic for the STM32h723 on the website. Can I get a reference schematic for this?

I need the STM32h723 reference schematic for the eMMC.

This topic has been closed for replies.

4 replies

Tesla DeLorean
Guru
April 10, 2023

They wire up like an SDMMC, should use series resistors.

Look at STM32H745I-DISCO schematic ​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
DHRyu
DHRyuAuthor
Associate
April 10, 2023

Thank you very much.

I would be grateful if you could tell me one more thing.

Does USB HS connection need to use PHY IC with ULPI interface?

waclawek.jan
Super User
April 10, 2023

USB HS peripheral in STM32 contains a built-in FS PHY, so if you are OK with communicating at FS (12MBit/s raw data rate), you don't need an external PHY.

JW

ST Technical Moderator
April 10, 2023

Hello @DHRyu​,

You can check the schematic of the Nucleo-H723, sheet 5 you can find out the SDMMC wiring and schematic of STM32H745I-DISCO for the eMMC.

It would be better to enter a new post for a new question to adhere to ST Community guidelines.

As referenced in Datasheet, section 3.43 Universal serial bus on-the-go high-speed (OTG_HS) 

When using the USB OTG_HS interface in HS mode, an external PHY device connected to the ULPI is required.

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL