Skip to main content
Associate II
Apr 4, 2024 8:06 AM UTC
Solved

Hwo to make simulation or HIL with stm32F407VET6 black board

Hi community.

I'm working with stm32F407VET6 black board, and I need to simulate the project before implementing it in the real system. so, I need a software simulation of stm32F407xx or how to make it in hardware in the loop, I tried to search for a library in proteus, but I don't find one for F407XX.

thanks. 

This topic has been closed for replies.
Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Apr 4, 2024 8:22 AM UTC

There is no simulator for STM32 because its complexity does not allow for a sensibly affordable solution.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

9 replies

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Apr 4, 2024 8:22 AM UTC

There is no simulator for STM32 because its complexity does not allow for a sensibly affordable solution.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
mƎALLEm
ST Technical Moderator
Apr 4, 2024 8:35 AM UTC

You need to contact Labcenter via this link: https://www.labcenter.com/contact/

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Andrew Neil
Super User
Apr 4, 2024 9:02 AM UTC

@toufik_iddou wrote:

how to make it in hardware in the loop,


So have you done any research into how "Hardware In the Loop" (HIL) testing is generally done?

The name says it all, really: You take your hardware, and you put it in your test loop!

So you will need:

  1. Computer-controlled stuff to supply the test conditions to your hardware;
  2. Computer-controlled stuff to monitor the outputs from your hardware;
  3. Probably also some monitoring/instrumentation interfaces in your hardware
  4. Software to automate your test.

None of this is specific to STM32.

 

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Associate II
Apr 10, 2024 11:50 PM UTC

I'll explain to you my idea and tell me if I can do it.
I need to control an inverter with stm32F407VET6 in closed loop the stm32 take the V_out of the inverter as input and produce a PWM signal as output to control the inverter.
I made the circuit of the inverter with proteus, but I don't have STM32F407 in proteus.
so, my idea is to connect my real stm32 and make a communication between them and proteus (I think that is the HIL)
am I right??

Andrew Neil
Super User
Apr 11, 2024 8:01 AM UTC

@toufik_iddou wrote:

 my idea is to connect my real stm32 and make a communication between them and proteus (I think that is the HIL)


Yes, that would indeed be "Hardware (your actual STM32) In your test Loop" - HIL

As for what facilities Proteus has to achieve that, you would need to study the Proteus documentation and/or contact Labcenter about that - it is nothing to do with ST:

https://www.labcenter.com/contact/

https://www.labcenter.com/help-center/

https://www.labcenter.com/tutorials/

https://support.labcenter.com/forums/

 


@toufik_iddou wrote:

 the stm32 take the V_out of the inverter as input ...


So you will need something to provide that voltage input to your UUT (Unit Under Test) - perhaps a controllable power supply, or a voltage-output DAC controlled from your test system (ef, Proteus).

 


@toufik_iddou wrote:

... and produce a PWM signal as output to control the inverter.


And you will need something else that can detect that signal, and feed it back into your test system.

 

Again, you're going to have to study the Proteus support resources (documentation, tutorials, etc) and/or contact Labcenter to find out what Proteus actually supports for this kind of stuff.

This is not a Proteus support forum.

 

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.