Skip to main content
JKim.2
Associate III
Mar 31, 2025 5:58 AM UTC
Solved

how to set variable latency or fixed latency for Octo-SPI PSRAM on STM32L4P5G-DK board?

Hello,

OSPI_RegularCmdTypeDef in stm32l4xx_hal_ospi.h doesn't include ".LatencyMode" member as below.

how to set variable latency or fixed latency for Octo-SPI PSRAM on STM32L4P5G-DK board?

Thanks.

 

typedef struct

{

uint32_t OperationType; /*!< It indicates if the configuration applies to the common registers or

to the registers for the write operation (these registers are only

used for memory-mapped mode).

This parameter can be a value of @ref OSPI_OperationType */

uint32_t FlashId; /*!< It indicates which external device is selected for this command (it

applies only if Dualquad is disabled in the initialization structure).

This parameter can be a value of @ref OSPI_FlashID */

uint32_t Instruction; /*!< It contains the instruction to be sent to the device.

This parameter can be a value between 0 and 0xFFFFFFFF */

uint32_t InstructionMode; /*!< It indicates the mode of the instruction.

This parameter can be a value of @ref OSPI_InstructionMode */

uint32_t InstructionSize; /*!< It indicates the size of the instruction.

This parameter can be a value of @ref OSPI_InstructionSize */

uint32_t InstructionDtrMode; /*!< It enables or not the DTR mode for the instruction phase.

This parameter can be a value of @ref OSPI_InstructionDtrMode */

uint32_t Address; /*!< It contains the address to be sent to the device.

This parameter can be a value between 0 and 0xFFFFFFFF */

uint32_t AddressMode; /*!< It indicates the mode of the address.

This parameter can be a value of @ref OSPI_AddressMode */

uint32_t AddressSize; /*!< It indicates the size of the address.

This parameter can be a value of @ref OSPI_AddressSize */

uint32_t AddressDtrMode; /*!< It enables or not the DTR mode for the address phase.

This parameter can be a value of @ref OSPI_AddressDtrMode */

uint32_t AlternateBytes; /*!< It contains the alternate bytes to be sent to the device.

This parameter can be a value between 0 and 0xFFFFFFFF */

uint32_t AlternateBytesMode; /*!< It indicates the mode of the alternate bytes.

This parameter can be a value of @ref OSPI_AlternateBytesMode */

uint32_t AlternateBytesSize; /*!< It indicates the size of the alternate bytes.

This parameter can be a value of @ref OSPI_AlternateBytesSize */

uint32_t AlternateBytesDtrMode; /*!< It enables or not the DTR mode for the alternate bytes phase.

This parameter can be a value of @ref OSPI_AlternateBytesDtrMode */

uint32_t DataMode; /*!< It indicates the mode of the data.

This parameter can be a value of @ref OSPI_DataMode */

uint32_t NbData; /*!< It indicates the number of data transferred with this command.

This field is only used for indirect mode.

This parameter can be a value between 1 and 0xFFFFFFFF */

uint32_t DataDtrMode; /*!< It enables or not the DTR mode for the data phase.

This parameter can be a value of @ref OSPI_DataDtrMode */

uint32_t DummyCycles; /*!< It indicates the number of dummy cycles inserted before data phase.

This parameter can be a value between 0 and 31 */

uint32_t DQSMode; /*!< It enables or not the data strobe management.

This parameter can be a value of @ref OSPI_DQSMode */

uint32_t SIOOMode; /*!< It enables or not the SIOO mode.

This parameter can be a value of @ref OSPI_SIOOMode */

} OSPI_RegularCmdTypeDef;

This topic has been closed for replies.
KDJEM.1
KDJEM.1Best answer
ST Technical Moderator
Apr 14, 2025 7:04 AM UTC

Hello @JKim.2,

 

Thank you for updating post.

To clarify my last reply, the latency is not available when Octo-SPI or Quad-SPI mode is selected. Because the latency is supported with hyperBus protocol. The latency can be configured via the OCTOSPI HyperBus latency configuration register (OCTOSPI_HLCR). The reset value is 0x0000 0000.

KDJEM1_0-1744613615241.png

 

->The AN5050 defines the latency mode for octal-spi PSRAM as "N/A". So, how can I know the default mode?

In AN5050, the mode using with PSRAM APS1604M-3SQR is the Quad-SPI mode and the mode using with PSRAM APS6408L-30B-BA is Octo-SPI mode.

 

 

KDJEM1_2-1744614129143.png

 

You can choose the mode depending on memory datasheet.

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.

3 replies

KDJEM.1
ST Technical Moderator
Apr 9, 2025 9:26 AM UTC

Hello @JKim.2,

 

The latency is supported with hyperBus protocol as mentioned in reference manual section 19.4.5 HyperBus protocol.

 

To configure the PSRAM on STM32L4P5G-DK board, I recommend you to follow AN5050 section 7 OCTOSPI application examples.

 

KDJEM1_0-1744190665872.png

KDJEM1_1-1744190719354.png

 

I hope this help you.

Thank you.

Kaouthar

 

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.
JKim.2
JKim.2Author
Associate III
Apr 14, 2025 1:46 AM UTC

Hello @KDJEM.1 ,

 

The AN5050 defines the latency mode for octal-spi PSRAM as "N/A". So, how can I know the default mode?

 

Thanks.

KDJEM.1
KDJEM.1Best answer
ST Technical Moderator
Apr 14, 2025 7:04 AM UTC

Hello @JKim.2,

 

Thank you for updating post.

To clarify my last reply, the latency is not available when Octo-SPI or Quad-SPI mode is selected. Because the latency is supported with hyperBus protocol. The latency can be configured via the OCTOSPI HyperBus latency configuration register (OCTOSPI_HLCR). The reset value is 0x0000 0000.

KDJEM1_0-1744613615241.png

 

->The AN5050 defines the latency mode for octal-spi PSRAM as "N/A". So, how can I know the default mode?

In AN5050, the mode using with PSRAM APS1604M-3SQR is the Quad-SPI mode and the mode using with PSRAM APS6408L-30B-BA is Octo-SPI mode.

 

 

KDJEM1_2-1744614129143.png

 

You can choose the mode depending on memory datasheet.

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.