Skip to main content
Bogdan
Senior
February 1, 2023
Solved

How to power STM32H725IGK6

Hello,

i intend to use a STM32H725IGK6 device in my design.

The system will be suplied from a single 3.3 voltage source.

Apart from VDD,VBAT pins, i see this device has some VDDLDO pins, and 3 VCAP pins.

How shall i power the vddldo pins? Can i tie them together with VDD supply ( 3.3V) ?

As i understood the vddLDO pins is supling the internal core regulator.

And what about the VCAP pins? All 3 vcap pins must be connecter together with capacitor to ground? Or every vcap pin separate tied to GND via capacitor?

This topic has been closed for replies.
Bogdan
BogdanBest answer
Senior
February 24, 2023

Hello,

thank you very much for the answers, i have left the vcap pins independent, each with its own 2.2uf capacitor.

I am not using the internal SMPS module ( i already managed to brik8 2-3 mcu's:beaming_face_with_smiling_eyes: because of that) .

3V3 is suplied directly to the LDO input pins, and everything seems to work well

4 replies

Piranha
Principal III
February 1, 2023

Read the AN5419.

ChahinezC
Associate II
February 2, 2023

Hello @Bogdan​,

As @Piranha​ mentioned, I recommend you referring to the "Power supplies" section of the AN5419 and for your design based on the STM32H725 you can check the Power supply decoupling of the "Recommended PCB routing guidelines for STM32H723/733, STM32H725/735 and STM32H730 microcontrollers" section.

Regards,

Chahinez.

LCE
Principal III
February 2, 2023

... and in case of doubt have a look at the schematics of the dev boards for that series, like the H723 Nucleo or the H735 Discovery Kit.

Bogdan
BogdanAuthorBest answer
Senior
February 24, 2023

Hello,

thank you very much for the answers, i have left the vcap pins independent, each with its own 2.2uf capacitor.

I am not using the internal SMPS module ( i already managed to brik8 2-3 mcu's:beaming_face_with_smiling_eyes: because of that) .

3V3 is suplied directly to the LDO input pins, and everything seems to work well