Skip to main content
ijona
Associate II
June 26, 2019
Question

How to downgrade/restore STlinkv2 ?

  • June 26, 2019
  • 14 replies
  • 4477 views

Hi,

I update my STlinkv2 from V2J29M18 to V2J34M25 firmware version and i lost the UART communication.

I have two STlinkV2 and one is always in V2J29M18 version so i'm sure that the problem come from the update.

So my question is how i can restore the V2J29M18 firmware ? (the easy way i think)

Or how to re-active the UART communication with the V2J34M25 version ?

Best regards.

This topic has been closed for replies.

14 replies

Tesla DeLorean
Guru
June 26, 2019

Fiddled with any of the other upgrade check boxes?

Get an older version of the ST-LINK Utilities or stand alone upgrade tool you used to put V2J29 on it and use that again to downgrade.

Version 2.28.18

https://drive.google.com/open?id=0B7OY5pub_GfIM21yTDZvcmNKQUk

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
S C
ST Employee
June 27, 2019

Hello,

May you please detail on which board exactly you faced the issue, and the overall context (host PC and target application) ? The ST-Link/V2 is the name of the standalone probe which does not provide UART connection so you are most probably mentioning a disco/nucleo/eval board embedding the ST-Link/V2-1. On those boards, the VCP initialization changed in version V2J33M25: prior to this version, the VCP was initialized at ST-Link startup, with arbitrary default parameters (9600 bauds, ...), which created issues in some cases. Since V2J33M25, the VCP is initialized when the host issues a SET_LINE_CODING command, which is the command configuring the VCP (sent by host terminal applications). I guess your issue is somehow related to this change but I would need more information to better understand your case.

ijona
ijonaAuthor
Associate II
June 27, 2019

Hi S C,

I use a custom probe where i recycling the IC from a nucleo L011K4. But the configuration of my probe is close to the nucleo.

So I have not yet tested with an original nucleo board.

What is VCP ? i think this is the key because my probe work for programming and debug mode.

S C
ST Employee
June 27, 2019

VCP stands for Virtual Com Port: briefly it's a gateway USB to UART, allowing to communicate to a target UART through the ST-Link USB channel. On Nucleo boards (like any other ST-Link/V2-1 based board), an UART of the STM32F103CB of the ST-Link is connected to an UART of the target. If you don't activate the VCP, the ST-Link firmware V2J34M25 (and later) activates a pull-up on its Tx pin (Rx for target) and let its Rx pin floating (while previously, a pull-up was also activated on this pin, because of VCP activation). This is perhaps what explains the regression in your case

ijona
ijonaAuthor
Associate II
June 27, 2019

Ok so how i can activate the VCP ?

S C
ST Employee
June 27, 2019

You may use applications like Putty or teraterm, for investigations. But your application should work without the ST-Link VCP activated; I still don't understand what you mean by "I lost the UART communication", I initially thought you spoke about the UART of the ST-Link VCP. If it's not the case, perhaps you also need to check the hardware configuration of your UART communication, which perhaps requires a pull-up at least on one side, instead of relying on the ST-Link configuration ?

ijona
ijonaAuthor
Associate II
June 27, 2019

So when i place a jumper between the Tx-Rx of my probe i can receive an echo (same behavior on new and old firmware)

ijona
ijonaAuthor
Associate II
June 27, 2019

Sorry i send a response before your question...

So my problem is i can't receive any trace on my terminal from the device with my probe flashed with the new firmware (V2J34M25).

If connect a probe with a firmware under V2J33... all is ok.

Terminal stay clear with the new firmware (of the probe). No invalid characters or garbage it's just open and clear.

S C
ST Employee
June 27, 2019

My understanding is that you connect the target UART to a terminal but in the same time you kept the connection to the ST-Link UART, is that right ? In that case I suggest you to activate the pull-up on the target UART_Tx pin and then it should work even with recent probe firmware versions

ijona
ijonaAuthor
Associate II
June 27, 2019

I have tested with an old nucleo STM32L432KC to upgrade the ST-Link firmware and it's work fine.

So i also try to add a physical pull-up on Tx (and Rx) but no effect. I check with my oscilloscope the Tx Rx line with the old and the new probe it's same signal.

I think on nucleo board it's have a bride connected what isn't on my probe i need to double check this.