Skip to main content
JGast.2
Associate
May 23, 2023
Question

How many HW breakpoints does STLINK-V3 family have? I'm interested on STLINK-V3MINIE

..

This topic has been closed for replies.

3 replies

Tesla DeLorean
Guru
May 23, 2023

Probably whatever the MCU facilitates via FPB units.

I don't think they offer "Flash Break Points" in the Segger sense.

You could also use a Break Point function (use a checkpoint code, or __FILE__,__LINE__), or explicitly place BKPT # instructions. Perhaps gate those with a flag variable so you can run the exact same code in release/debug conditions.

Use instrumentation to determine dynamic flow.

Dead-stopping some machines can cause catastrophic damage, you learn to approach things differently..

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
JGast.2
JGast.2Author
Associate
May 23, 2023

I understand your point, runtime debugging is always available, but i'm looking for HW capabilities, knowing that they "break" the program.

So you mean it all depends on the MCUs embedded comparators? STLINK does not provide HW breakpoints itself?

AScha.3
Super User
May 23, 2023

AFAIK..

The ARM cores have different complexity, from simple F0 to H7 or F7​, and so are the integrated co-processors, the debug units.

See ARM documents about cores and debug capabilities..

So the hardware debug capabilities are fixed with your choice of core.

Big core has big debug units...

​

If you feel a post has answered your question, please click on " Best Answer ".