Skip to main content
JRich.7
Associate II
April 1, 2022
Solved

How can I print to a terminal on my PC via UART?

Hi all,

I've tried every example I can find to send data to a terminal using UART on my Nucleo 144. Every time the code builds fine but there is never anything on the terminal, and the code doesn't get stuck anywhere it runs fine.

This topic has been closed for replies.
Guenael Cadier
Guenael CadierBest answer
ST Employee
April 1, 2022

On this Nucleo board, communication between the target STM32L5

and the ST-LINK is enabled using LPUART1, to support the Virtual COM port.

Associated GPIO are as in your hal msp file PG7 and PG8 for TX/RX.

Is your terminal configured in same way than your LPUART1 (BaudRate = 209700; WordLength 7Bits, 1 StopBit, No Parity) ?

Default value used by MX for baudrate might need to be updated, depending on how is configured your hyperterminal open on Virtual COM port ...

Regards

4 replies

Guenael Cadier
ST Employee
April 1, 2022

Hello @JRich.7​ 

What nucleo board are you using ?

If you generate your project using CubeMX, TX/RX pins associated to the U(S)ART instance you are using, are expected to be initialised in the stm32XXxx_hal_msp.c file (in the HAL_UART_MspInit() function). Please make sure these GPIO are corresponding to those you expect to use on your Nucleo board.

Are you connecting your board to the terminal using VCP ?

Regards

JRich.7
JRich.7Author
Associate II
April 1, 2022

I'm using L4R5ZI-P. I'll attach the HAL_UART_MspInit() function below, I think it's correct but not sure how to be certain. I've tried both using a command shell console within CubeIDE and also with PuTTY. Thanks for your help!

/**
* @brief UART MSP Initialization
* This function configures the hardware resources used in this example
* @param huart: UART handle pointer
* @retval None
*/
void HAL_UART_MspInit(UART_HandleTypeDef* huart)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
 RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};
 if(huart->Instance==LPUART1)
 {
 /* USER CODE BEGIN LPUART1_MspInit 0 */
 
 /* USER CODE END LPUART1_MspInit 0 */
 /** Initializes the peripherals clock
 */
 PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_LPUART1;
 PeriphClkInit.Lpuart1ClockSelection = RCC_LPUART1CLKSOURCE_PCLK1;
 if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
 {
 Error_Handler();
 }
 
 /* Peripheral clock enable */
 __HAL_RCC_LPUART1_CLK_ENABLE();
 
 __HAL_RCC_GPIOG_CLK_ENABLE();
 HAL_PWREx_EnableVddIO2();
 /**LPUART1 GPIO Configuration
 PG7 ------> LPUART1_TX
 PG8 ------> LPUART1_RX
 */
 GPIO_InitStruct.Pin = GPIO_PIN_7|GPIO_PIN_8;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
 GPIO_InitStruct.Alternate = GPIO_AF8_LPUART1;
 HAL_GPIO_Init(GPIOG, &GPIO_InitStruct);
 
 /* USER CODE BEGIN LPUART1_MspInit 1 */
 
 /* USER CODE END LPUART1_MspInit 1 */
 }
 else if(huart->Instance==USART2)
 {
 /* USER CODE BEGIN USART2_MspInit 0 */
 
 /* USER CODE END USART2_MspInit 0 */
 
 /** Initializes the peripherals clock
 */
 PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_USART2;
 PeriphClkInit.Usart2ClockSelection = RCC_USART2CLKSOURCE_PCLK1;
 if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
 {
 Error_Handler();
 }
 
 /* Peripheral clock enable */
 __HAL_RCC_USART2_CLK_ENABLE();
 
 __HAL_RCC_GPIOD_CLK_ENABLE();
 /**USART2 GPIO Configuration
 PD3 ------> USART2_CTS
 PD4 ------> USART2_RTS
 PD5 ------> USART2_TX
 PD6 ------> USART2_RX
 */
 GPIO_InitStruct.Pin = GPIO_PIN_3|GPIO_PIN_4|GPIO_PIN_5|GPIO_PIN_6;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
 GPIO_InitStruct.Alternate = GPIO_AF7_USART2;
 HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);
 
 /* USER CODE BEGIN USART2_MspInit 1 */
 
 /* USER CODE END USART2_MspInit 1 */
 }
 else if(huart->Instance==USART3)
 {
 /* USER CODE BEGIN USART3_MspInit 0 */
 
 /* USER CODE END USART3_MspInit 0 */
 
 /** Initializes the peripherals clock
 */
 PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_USART3;
 PeriphClkInit.Usart3ClockSelection = RCC_USART3CLKSOURCE_PCLK1;
 if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
 {
 Error_Handler();
 }
 
 /* Peripheral clock enable */
 __HAL_RCC_USART3_CLK_ENABLE();
 
 __HAL_RCC_GPIOC_CLK_ENABLE();
 /**USART3 GPIO Configuration
 PC4 ------> USART3_TX
 PC5 ------> USART3_RX
 */
 GPIO_InitStruct.Pin = GPIO_PIN_4|GPIO_PIN_5;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
 GPIO_InitStruct.Alternate = GPIO_AF7_USART3;
 HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
 
 /* USER CODE BEGIN USART3_MspInit 1 */
 
 /* USER CODE END USART3_MspInit 1 */
 }
 
}

Guenael Cadier
Guenael CadierBest answer
ST Employee
April 1, 2022

On this Nucleo board, communication between the target STM32L5

and the ST-LINK is enabled using LPUART1, to support the Virtual COM port.

Associated GPIO are as in your hal msp file PG7 and PG8 for TX/RX.

Is your terminal configured in same way than your LPUART1 (BaudRate = 209700; WordLength 7Bits, 1 StopBit, No Parity) ?

Default value used by MX for baudrate might need to be updated, depending on how is configured your hyperterminal open on Virtual COM port ...

Regards

JRich.7
JRich.7Author
Associate II
April 1, 2022

Thank you! That fixed it :D