Skip to main content
ASORB.1
Visitor II
April 19, 2022
Question

Hi, I installed the driver dpinst_x86.exe of STSW-LINK009 package on INTEL i5 hardware platform and Windows 11 SO and it doesn't work!

Please, can I install the ST-LINK, ST-LINK/V2, ST-LINK/V2-1, STLINK-V3 USB driver dpinst_amd64.exe signed for windows 10 on INTEL i5 hardware platform and Windows 11 SO?

Thanks in advance

Angelo Sorbo

This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
April 19, 2022

Not really Microsoft IT team here.

But can't you go into Device Manager, select the device and get it to Upgrade to a more suitable driver you furnish? Should be able to unpack the .ZIP to a real directory, and then point Windows at it in the "I've got a driver" sense.

You can also run the dpinst too, but Device Manager, or running the .INF should also be options.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..