Skip to main content
mat.osz.546949133819912E12
Visitor II
January 8, 2019
Question

HardRst command not working with latest STM Utility

  • January 8, 2019
  • 3 replies
  • 1177 views

Hello,

after update Stm32 Utility to version 4.3.0 HardRst command stopped working.

In log I can see:

-HardRst is available only on ST-LINK/V2 with firmware V2J12S3 and later.

but I have connected ST-LINK V2 with V2.J32.S7 firmware.

This topic has been closed for replies.

3 replies

erikilainen
Visitor II
February 26, 2019

I had the same problem.

I tried both upgrade and downgrade of ST-LINK/V2 FW but it did not help.

Installed Stm32 Utility v4.1.0 and now it works

There is a suspicious "new feature" in release notes for v4.2.0:

  • Add support of hard reset pulse feature in command line interface (CLI)

olivier
Associate
July 22, 2020

This is still not fixed in 4.5.0. Can we expect a fix soon?

WMahr.1
Visitor II
February 9, 2021

Unfortunate this is still not fixed in 4.6.0. :(

I am currently use -RST combined with -C Hrst or -C UR. As far as I can see the main difference is that this command does a device connect first.