Skip to main content
Associate II
December 29, 2024
Solved

Getting started with NUCLEO-H7S3L8 USB

Hi,

I'm trying to get started with the STM32 NUCLEO-H7S3L8 board to create a USB HS device. I am new to the boot/application split development (also to trustzone) and don't know where to find the right resources to get started. I have tried using the STM32CubeIDE examples importer but keep receiving "failed to copy error" which I don't know how to debug. I have also tried loading the project from the git repo, I can compile and run the boot project but know how to properly setup the application project to run as well.

I would really appreciate some pointers on where to find the information to get the CDC_Standalone example running and how to develop with the boot and application.

Apologies I can't be more specific, I seem a little out of my depth and don't know where to start!

This topic has been closed for replies.
LinduriBest answer
Associate II
January 14, 2025

After reading around for a considerable time I discovered that the STMCube code generator always sets the USB reference clock to 24MHz (unfortunately I have mis-placed the link to the post) which then conflicts with the HAL USB Init.

The problem was fixed by setting the USBPHYC Clock Mux to use the NUCELO-H7S3L8 external 24MHz HSE.

7 replies

ST Employee
December 30, 2024
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Pavel A.
December 30, 2024

In addition to the links above, here you can help and support with your STM32 project.

https://www.fiverr.com/categories/programming-tech/electronics-engineering/embedded-systems-iot?ref=platform%3Astm32

 

LinduriAuthorBest answer
Associate II
January 14, 2025

After reading around for a considerable time I discovered that the STMCube code generator always sets the USB reference clock to 24MHz (unfortunately I have mis-placed the link to the post) which then conflicts with the HAL USB Init.

The problem was fixed by setting the USBPHYC Clock Mux to use the NUCELO-H7S3L8 external 24MHz HSE.

Senior
February 16, 2025

Hello @Linduri,

Could you please share your minimal working USB Device ioc file if possible ?

I am trying to setting it up without success...

Thanks,

s.

LinduriAuthor
Associate II
February 17, 2025

After further communication with ST they helped me diagnosed that I had failed to correctly enable the internal USB power regulator. I have attached the minimal IOC for your convenience.

Senior
February 17, 2025

Thanks, @Linduri.

My setup is quiet different, taken from the CDC_Standalone.ioc example, so booting from external flash and USB HS Device. I also think that UCPD setup is required for this purpose (CDC_Standalone.ioc enables it by default).

I will also test yours.

s.