Skip to main content
Rami Rosenbaum (old)
Associate III
May 29, 2017 12:01 PM UTC
Solved

Flashing boot-loader, production-data and application

Posted on May 29, 2017 at 14:01

hi,

I'm working on a project, on a stm32F101.

The product is a proprietary boot-loader and application (which can be updated later on, via the BL).

I'll need to hold some production-data, serial-number, etc, less than 256 bytes.

I'm short in storage, don't want to waste a whole sector.

I want to hold it in a known location, for the application to read, say address 0x08000100, enough for the boot-loader vector-table.

I'm trying to flash the 3 via ST-Link Utility command-line interface, but they erase one another.

How can I Skip Flash Erase?

I'm flashing the boot-loader:

ST-LINK_CLI.exe -c SWD -P BootLoader.hex -V

I'm flashing the serial-number:

ST-LINK_CLI.exe -c SWD -P SerialNumber.bin 0x08000100 -V

I'm flashing the application:

ST-LINK_CLI.exe -c SWD -P Application.bin 0x08008000 -V

My additions to boot-loader linker script:

define symbol __ICFEDIT_intvec_start__                = 0x08000000;

define symbol __ICFEDIT_region_ROM_PRODUCTION_start__ = 0x08000100;

define symbol __ICFEDIT_region_ROM_PRODUCTION_end__   = 0x080001FF;

define symbol __ICFEDIT_AppHeader_start__             = 0x08000200;

define symbol __ICFEDIT_region_ROM1_start__           = 0x08000000;

define symbol __ICFEDIT_region_ROM1_end__             = 0x080000FF;

define symbol __ICFEDIT_region_ROM2_start__           = 0x08000200;

define symbol __ICFEDIT_region_ROM2_end__             = 0x0801FFFF;

define region ROM_region     = mem:[from __ICFEDIT_region_ROM1_start__ to __ICFEDIT_region_ROM1_end__] | mem:[from __ICFEDIT_region_ROM2_start__ to __ICFEDIT_region_ROM2_end__];

define region ROM_production = mem:[from __ICFEDIT_region_ROM_PRODUCTION_start__ to __ICFEDIT_region_ROM_PRODUCTION_end__];

Thanks

#linker-script #st-link-utility
This topic has been closed for replies.
Jeroen3
Jeroen3Best answer
Senior
May 29, 2017 2:22 PM UTC
Posted on May 29, 2017 at 16:22

With -w8 ?

You do know have to erase flash to program 1's. You can only program 0's.

8 replies

Jeroen3
Jeroen3Best answer
Senior
May 29, 2017 2:22 PM UTC
Posted on May 29, 2017 at 16:22

With -w8 ?

You do know have to erase flash to program 1's. You can only program 0's.

Rami Rosenbaum (old)
Associate III
May 29, 2017 4:31 PM UTC
Posted on May 29, 2017 at 16:31

-w8/-w32 writes 1/4 bytes to flash.

Easier for me to write the full serial-number with

-P SerialNumber.bin

, after all, the SN is generated by a production-tool.

But - that's not the issue, I didn't write the flash driver, I only have the ST-LINK_CLI.exe interface...

How should I use it correctly?

Tesla DeLorean
Guru
May 29, 2017 7:19 PM UTC
Posted on May 29, 2017 at 19:19

Can you have the serializer, or other app, combine the .hex and .bin into a singular .hex that's burned in one operation?

Can't say I've battled my way through the ST-LINK command line.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..