Skip to main content
FrankNatoli
Associate III
May 13, 2023
Question

Failure to convert ST-LINK to J-LINK

STM offers a utility to convert an ST-LINK debugger to J-LINK debugger.

USB drivers are current.

But when "stlinkreflash.exe" is run [in admin mode], it says "cannot find an ST-LINK, multiple ST-LINKs are plugged in, or ST-LINK in use".

None of that is true.

After exiting "stlinkreflsh.exe", IAR has no problem finding and burning the ST-LINK STM32H7B3I DK board.

Device Manager clearly shows only one ST-LINK is present.

No other process is running that touches the ST-LINK.

What does it take to please "stlinkreflash.exe"?

I need J-LINK feature to breakpoint on memory write to help identify corruption caused by STM USB host driver.

This topic has been closed for replies.

5 replies

AScha.3
Super User
May 13, 2023

 STM32H7B3I DK --> V3E is integrated into the board

the ST-LINK to J-LINK works only for stLink V2.1 - afaik.

i did it on a STM32F072B-DISCO board, working ok. just - every day you get at first use a window, to tell you, this is a demo version and you should buy some segger products...

If you feel a post has answered your question, please click on " Best Answer ".
FrankNatoli
Associate III
May 13, 2023

Well, thanks.

Humorously, I have two Segger J-Links, but they cannot be attached to a STM32H7B3I DK board.

I also have a STM32H7B3I EVAL board, to which a Segger can be attached, but I can't get the STM USB Host driver to recognize the mouse, neither on the OTG FS port nor the OTG HS port.

The DK board is recognizing the mouse, but the STM USB Host driver is corrupting queue structures, and I can't breakpoint on memory write with the ST-LINK debugger.

AScha.3
Super User
May 13, 2023

>I have two Segger J-Links, but they cannot be attached to a STM32H7B3I DK

why ?? (or are this copies - with old firmware ?)

If you feel a post has answered your question, please click on " Best Answer ".