Skip to main content
Franckeno
Associate
February 1, 2022
Question

Failed to start GDB server

Hello, I have been trying for a while to test the STMCube programming chain up to the STM32F411 via the STLink without success despite all the ideas read in the forum. During a review of the requirements for the installation of CUBE it is noted, under Windows, WIN 7, 10 but not 8 or 8.1. Too bad, 8.1 is my OS. I attach the error message that it returns to me systematically. Thanks for your help !

Error in final launch sequence: Failed to start GDB server

Error in initializing ST-LINK device.

Reason: (17) Could not find an ST-LINK with serial number 310061000E00004637364D4E.

Please verify the serial number in the debug c

PS: the serial number is the same as the one present when opening STM32 LINK utility

This topic has been closed for replies.

2 replies

Mike_ST
ST Technical Moderator
February 1, 2022

Hello

It is an STM32F411 Discovery board ?

Can you connect to the F411 with the ST-Link Utility ?

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 
Franckeno
FranckenoAuthor
Associate
February 4, 2022

Hello, no I am using STM32f411 black pill. And yes I can connect without problem with STM Link utility. Have a nice day and thank you