Skip to main content
Lachie
Associate
April 16, 2020
Question

"Failed to list debug probes" when scanning for ST-LINK S/N

STM32 Cube IDE throws failure message "Failed to list debug probes" when scanning for ST-LINK S/N under Debug Configurations/Debugger/GDB Server Command Line Options/Interface.

Problem has presented itself in last hour. It was working with a Nucleo-F042K6 and now not working with either the Nucelo-F042K6 and a Nucleo-F746ZG.

Trying to debug code that incorporates FreeRTOS Middleware utilising CMSIS_V2 hence the move to the significantly more powerful Nucleo-F746ZG as I realised RTOS is not compatible with the Nucelo-F042K6.

Ran ST-LINK Upgrade successfully on both boards.

Code compiled and downloaded from online mbed compiler works so I expect it is not an issue with the board.

Any assitance would be greatly appreciated.

This topic has been closed for replies.

1 reply

Lachie
LachieAuthor
Associate
April 20, 2020

Problem found to be Avast Antivirus, uninstalling STM32 Cube IDE and Avast and then reinstalling STM32 Cube IDE fixed the problem.