Skip to main content
Manny12
Associate II
October 14, 2022
Solved

F401C barebone, minimum circuit.

Hi

I'm new to STM32, I'm jumping from Arduino, and I'm out of my depth, perhaps I can humbly ask for some help.

I've done basic projects with the Nucleo board, and I wanted to give a try with a simple code on a barebone chip

I have this STM32F401CBU6 on UFQFPN-48, mounted on a Proto-Advantage SMT to Breadboard adapter, naked, just the MCU, no decoupling capacitors, pull-down resistors, etc., just naked.

I intend to put it on my breadboard, power it with a 3.3V Power Supply, and program it to blink a LED.

The code will be written with the CubeIDE and loaded via a Nucleo 64 reference board UM1724, which has an integrated STLink that according to the documentation, can be decoupled for the onboard STM32 target (by removing some header pins) and then used to program an external STM32 via SWD

Chapter 3.13 of the IC F401xB datasheet (that is the external MCU I'm using) talks about the power scheme, and I was wondering:

To just power on the MCU and receive SDW program, do I need to provide power to all VDDs or just VBAT?

What would be the bare minimum circuit that would let me read/write registers, load firmware, etc?

I know, out of my depth, but perhaps I can find my way in this maze.

This topic has been closed for replies.
waclawek.jan
waclawek.janBest answer
Super User
October 16, 2022

> Put a 4-pin connector for programming/debug: Vdd, SWDIO, SWCLK and GND.

I would add NRST, too.

I would also think about the role of VDD - it may be a power connection, or it may be just so that the STLink can measure the target's VDD (which influences programming algorithm at low voltages, or with the galvanic-decoupled STLink it provides the required output level), or it may be unwanted (if both STLink and the target connects this pin to their respective power rails while both being powered from a different source).

You may want to put signals on this connector in a particular order, eg. as they are on the Nucleo board. Even if you want to put them to some other order, it's a good idea to place GND in between SWDIO and SWCLK, so that it shields one from the other if a flat cable is used.

Don't use long cables, 15 cm should be mostly it.

But if you don't intend to build a PCB, just use the breadboard, these remarks are not that important.

OTOH, I hate solderless breadboards and recommend you to avoid them.

> Pull BOOT1 low with 100k.

BOOT1 = PB2, see datasheet.

As long as you don't intend to use the bootloader, just ground BOOT0 and you can forget about BOOT1.

> didnt think about that, how easy/hard is it to spot a fake?

I don't know, I don't have first-hand experience. Based on what I read (including the link I gave and other related threads on that forum), some fakes are very convincingly looking. They may be OK for hobby use, but ST's tools understandably try to detect them and refuse to work with them.

JW

17 replies

Tesla DeLorean
Guru
October 14, 2022

The part has a Data Sheet, would help to read it, or at least skim the power and connectivity portions.

Expect to connect ALL power pins appropriately,ie VSS's to ground VDD/VBAT to 3.3V. The VDDA runs the PLL and power-on-reset regardless of you're using ADC, DAC, etc

VCAP pins need capacitors, either one 4u7 or two 2u2 depending on IC. Should see around 1.25V on this if chip is viable.

Don't need crystals or clocks, part starts running from internal oscillator.

NRST should have an internal pull-up. Should see 3.3V if viable.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Manny12
Manny12Author
Associate II
October 14, 2022

I've been reading the datasheet and I already made all connections for VDD/VBAT/VDDA with their corresponding decoupling capacitors, NRST to 3.3V (missed the VCAP capacitors at the beginning, but connected it later, it seems to need only one), but I got errors when loading my program from Cube IDE, so I went to CubeProgrammer and I was able to sometimes connect to the target, read registers, etc, and sometimes not, and I didn't get the pattern. I was trying to erase the whole chip but some registers didn't let me (protected?), then I tried to change them but the programmer threw errors when I tried removing the protection. I couldn't make more sense of it, so I was looking for a more barebone setup, to simplify and troubleshoot because I thought my barebone setup had just too many wires around. I will take everything apart and wire it again and see what I missed. Hopefully, I didn't fry the MCU with an incorrect connection.

ONadr.1
Senior III
October 14, 2022

I think, that you need PCB for construction with STM32. They ned weeeery good grounding and blocked capacitors as well. Use STM32 on some breadboard si similar, like driving a lamborghini down a muddy forest road.

You can use the Nucleo module without programer (it is possible to cut it out) as a CPU brick to your own construction.

Manny12
Manny12Author
Associate II
October 14, 2022

I did order a PCB, from JLCPCB. With a design made in KiCAD, following a tutorial from Phil Salmony on YouTube, I pretty much replicated his design and added one more 4-pin header to use GPIOs. That PCB is centered around an F103C8 (that's what JLCPCB had in stock).

I haven't gotten it yet, but since I have this other barebone PCB here, I thought I would give it a try and see if I could learn anything.

On every other design I have made I first put all the ICs on a breadboard first, then when I'm happy then I order the PCB, but in this case, since I'm basically copying Phil's design, I ventured to order the PCB without testing on a breadboard first.

I have the hope that I can make work the barebone chip I have here, on a breadboard, nothing fancy, it doesn't have to be perfect or super stable, I just want to see if I can flash it and do something basic.

This is for a hobby, not work, and I know many of you here are paid $$ for your time and your knowledge and I understand many don't want to waste time on these newbie questions. I'm sure that I will be able to ask smarter questions once I have this little thing running.

ONadr.1
Senior III
October 14, 2022

Yes, I am a hobbyist too. I use usualy whole nucleo board for prototype. This is not so expensive, stable and modular. I know, that is much more bigger then arduino mini and etc. But it usualy doesnt matter in prototype. Or you can use small Blue pill modules with 32F103 or 32F411 and program them wia STLink from Nucleo board.

Manny12
Manny12Author
Associate II
October 14, 2022

I just ordered a generic blue pill with an STM32F103C6T6 from Amazon, I'll get it on Sunday. That will help me rule out that I'm making a mistake in wiring/using the STLink part of the Nucleo 64 board I'm using for SWD. I still have hopes of making my barebone chip work though.

waclawek.jan
Super User
October 15, 2022

For 'F4xx hardware design, read AN4488. Don't forget about BOOTx pins.

Blue pills these days are almost guaranteed to contain a counterfeit chip.

JW

Manny12
Manny12Author
Associate II
October 15, 2022

I didnt think about that, how easy/hard is it to spot a fake?

Manny12
Manny12Author
Associate II
October 15, 2022

Schematics attached.

I read the datasheet a few times as some of you advised, and I came up with a minimalistic circuit.

Again, I just want to power on the naked MCU I have, boot it, and load a simple program via SWDIO/SWCLK pins. I made schematics on KiCAD for this. I'm doing this on a breadboard (I know, some might say it will not work, but I asked ST support, and they told me that if I make my connections ‘solid’, they don’t see a reason why it wouldn’t work)

There is something I don't understand, the datasheet seems to indicate that I need to connect the VREF+ somewhere, I think I understand that I should connect it to VDDA which in my UFQFPN-48 package I don't have as a separate pin (the datasheet on page 33/139 says that the pin 9 is VDDA/VREF+ and it says that pin 8 is VSSA/VREF- so I'm more confused now, looks like VREF+ and VDDA are the same pins, and after reading 'power supply scheme' on page 56/139, I decided to wire VREF+ to VDD, in a similar way as the rest of VDD and VBAT, with decoupling capacitors.

I also read the AN4448 (hardware development for STM32F4xxxx) and it says on pages 25/50 and 26/50, that the boot modes are selected by the state of BOOT0 and BOOT1, but I don't have BOOT1 (actually I couldn't find BOOT1 in any package for this MCU)

So, right now, I'm not sure if I'm wiring VREF+ correctly, and I'm not sure how to select each of the three boots modes with only BOOT0

My schematic is here, if anyone cares to review it and critique it, that would be nice.0693W00000Uo7m7QAB.jpg

Manny12
Manny12Author
Associate II
October 15, 2022

Forgot to say, I can power this with the 3.3V output from a Nucleo 64 board, or from a buck converter I have.

The buck converter is model DPS5005 fed by a 14.4V Li-ion 4S pack I made myself. Definitely not lab-grade, but perhaps enough.

These are the specs of the DPS5005:

---------

Input voltage: 6-55V

Output voltage: 0V-50.00V

Output current: 0-5.000A

Output power: 0-250W

Output voltage resolution: 0.01V

Output current resolution: 0.001A

Output Voltage accuracy: +/- (0.5% + 1 digit)

Output Current accuracy: +/- (0.5% + 2 digits)

gbm
Super User
October 16, 2022

Put a 4-pin connector for programming/debug: Vdd, SWDIO, SWCLK and GND.

You only need 2 boot modes - user Flash and system ROM, selected with BOOT0. Pull it low with 20..100k resistor. Pull BOOT1 low with 100k.

Put at least one LED on the board connected to some port pin. Think of serial port at least.

Still, it won't be any better than the BluePIll.

A good, cost-effective alternative to BluePill with Chinese STM32F103-alike chip is the BlackPill with (hopefully) real STM32F401 at < 3.5 USD. F401 has USB bootloader, so no other stuff (like ST-Link or USB-serial) is required to program it.

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice
Manny12
Manny12Author
Associate II
October 16, 2022

Ill add two more pins on the debug interface.

(Found my BOOT1 pin, as pointed out by another commenter here, the datasheet says it was PB2)

waclawek.jan
waclawek.janBest answer
Super User
October 16, 2022

> Put a 4-pin connector for programming/debug: Vdd, SWDIO, SWCLK and GND.

I would add NRST, too.

I would also think about the role of VDD - it may be a power connection, or it may be just so that the STLink can measure the target's VDD (which influences programming algorithm at low voltages, or with the galvanic-decoupled STLink it provides the required output level), or it may be unwanted (if both STLink and the target connects this pin to their respective power rails while both being powered from a different source).

You may want to put signals on this connector in a particular order, eg. as they are on the Nucleo board. Even if you want to put them to some other order, it's a good idea to place GND in between SWDIO and SWCLK, so that it shields one from the other if a flat cable is used.

Don't use long cables, 15 cm should be mostly it.

But if you don't intend to build a PCB, just use the breadboard, these remarks are not that important.

OTOH, I hate solderless breadboards and recommend you to avoid them.

> Pull BOOT1 low with 100k.

BOOT1 = PB2, see datasheet.

As long as you don't intend to use the bootloader, just ground BOOT0 and you can forget about BOOT1.

> didnt think about that, how easy/hard is it to spot a fake?

I don't know, I don't have first-hand experience. Based on what I read (including the link I gave and other related threads on that forum), some fakes are very convincingly looking. They may be OK for hobby use, but ST's tools understandably try to detect them and refuse to work with them.

JW

Manny12
Manny12Author
Associate II
October 16, 2022

NRST is there, I added a cap and a momentary switch. I will put them in the same order, with GND in between. I dont intend to do a PCB with this schematic, but Ill keep in mind your suggestion regarding length, etc.

ONadr.1
Senior III
October 17, 2022

If you have bad luck and MCU wil be a counterfeit, it is posible desold it and sold oriinal MCU.