Question
External Power Supply for STM32H7 Nucleo-144 (MB1364) via Arduino Connectors
Dear ST Support Team,
I am using the STM32H7 Nucleo-144 (MB1364) board mounted as a shield on my custom hardware board.
I would like to power the Nucleo board directly from my carrier board through the Arduino connectors.
Could you please confirm the following points?
- Is it possible to power the Nucleo board by supplying 5 V through the Arduino connector?
- Is it possible to power the Nucleo board by supplying 3.3 V through the Arduino connector?
- Are there any specific jumper settings, protections, or precautions that should be considered, particularly regarding the USB/ST-LINK power supply?
- What is the recommended method for powering the Nucleo board when it is integrated into a custom embedded system?
Thank you in advance for your support.