Skip to main content
Gianluca Costa
Associate II
October 8, 2018
Question

External Loader: ST-Link Utility and STM32CubeProgrammer issues

Hi,

I’m developing and external loader for ST-Link Utility and STM32CubeProgrammer.

My constrains/ requirements are:

  • STM32F091RBTx as uC
  • external lash on SPI: EN25Q40
  • SDK/IDE Atollic

I used (started from) the source code from STM32CubeProgrammer and the document UM0892.

After a lot of attempts I have a version/FW that run on STM32CubeProgrammer, and I’m able to erase, write and read the external flash.

The issues are:

1) Sometimes connecting, disconnecting and reconnecting the STM32CubeProgrammer to the ST-Link/v2 I receive this error::

“Error: flash loader C:\Program Files (x86)\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin/ExternalLoader/EN25Q40_MT447 cannot be loaded.�?

This if and only if a I erase or write the external flash before disconnecting and reconnecting, If a only read the external flash the error doesn’t arise (I can disconnecting and reconnecting without problems) . If I don’t disconnect the ST-Link/v2 all work fine i.e. I’m able to write, erase and read many times the external flash.

2) The same binary module (.stldr) that I use on STM32CubeProgrammer if used with ST-Link Utility doesn’t work, in detail, the ST-Link Utility load the model without error, I can erase the external flash (mass erase, sector erase) and also I can read the external flash (the read is more slowly than STM32CubeProgrammer ) but the  write operation fails, and example log is:

11:27:27 : Erasing external memory success.

11:29:07 : Timeout during flash programming

11:2 9:07 : Error occured during program operation!

11:29:29 : Unable to run On-Chip verification!

11:29:38 : External memory program canceled

Someone can help me to understand these issues or suggest me a way to debug the FW/module?

Thanks.

Gianluca Costa

This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
October 8, 2018

The ST-LINK Utilities are not receiving development efforts and have their own bugs and shortcomings.

​

Diagnosis of issues can be via telemetry on the serial port. Code should be tested independently within your own test framework before integration.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..