Skip to main content
Associate III
Dec 18, 2025 10:24 AM UTC
Question

Extend STM32N6570-DK with a WiFi module & Zephyr

Hello,

We need to add WiFi connectivity to an STM32N6570-DK board and run Zephyr on it.

Is that possible? Can you propose a solution? 

We have seen X-NUCLEO-67W61M1 expansion board that can work with STM32N6. But can that board be connected with the DK board? 

Thank you very much for any suggestion.

Regards.

4 replies

Andrew Neil
Super User
Dec 18, 2025 10:34 AM UTC

Of course it can - just connect appropriate pins for SPI, UART, GPIO ...

You will have to check the User Guides and/or schematics of both boards to find appropriate available pins.

  • User Guides will be on the 'Documentation' tabs of the respective Product Pages;
  • schematics will be on the 'CAD Resources' tabs
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
mtvAuthor
Associate III
Dec 18, 2025 11:41 AM UTC

Thank you for the quick response.

What about the software side? Any clue what would be needed to run zephyr?

Thanks 

Andrew Neil
Super User
Dec 18, 2025 11:56 AM UTC
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.