Eth failed to work after few minutes with CubeMx Configuration
- 2 replies
- 209 views
I am working with STM32H747I -DISCO board
I am using CubeMx version 6.15, firmware: H7_V1.12.2, Freertos CMSIS2 - V10.3.1
configuration 1 : Generating from touchgfx and configuring Eth other all parameters commented in code (Touchgfx parameters).
Here ETH is working fine
configuration 2 : only configuring ETH with same configurating as above but generating from cubemx
Here Eth Communication worked for abt 10 to 20 min and then MCU stucked.
I compared both projects : it's all same (MPU configuration Linker script DMA Descriptor and RAM Heap pointer) ...middleware package, CMSIS files, Freertos config files, Lwip folder(lwip.c .h and ethernetif.c and lwipopt.h),LAN files all are same but still I am facing this issue.
I have attached wireshark snip when MCU got stucked
and IOC files 1. Touchgfx generated 2. CubeMx Generated