Skip to main content
DBurr
Senior
May 26, 2020
Question

Error when trying to debug code on custom board with ST-Link V3

Hi,

I have a custom board and am trying to debug live code on the target MCU with STM32CubeIDE but constantly getting the below error. I should note that I'm running Ubuntu 18.04 and have so far been successful in loading my built code with STM32CubeProgrammer and the same ST-Link V3 JTAG adaptor so I know that the JTAG port is working but STM32CubeIDE is not happy using it. I've also successfully debugged live code on a Nucleo dev board.

STMicroelectronics ST-LINK GDB server. Version 5.5.0
Copyright (c) 2019, STMicroelectronics. All rights reserved.
 
Starting server with the following options:
 Persistent Mode : Disabled
 Logging Level : 1
 Listen Port Number : 61234
 Status Refresh Delay : 15s
 Verbose Mode : Disabled
 
Waiting for debugger connection...
Debugger connected
 -------------------------------------------------------------------
 STM32CubeProgrammer v2.4.0 
 -------------------------------------------------------------------
 
ST-LINK SN : 003D00253038511834333935
ST-LINK FW : V3J6M2B4S1
Voltage : 3.31V
Error: ST-LINK error (DEV_UNKNOWN_MCU_TARGET)
2nd connect tentative with a lower frequency (8MHz)
ST-LINK SN : 003D00253038511834333935
ST-LINK FW : V3J6M2B4S1
Voltage : 3.31V
Error: ST-LINK error (DEV_UNKNOWN_MCU_TARGET)
Encountered Error when opening /opt/st/stm32cubeide_1.1.0/plugins/com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.linux64_1.3.0.202002181050/tools/bin/STM32_Programmer_CLI
Error in STM32CubeProgrammer
Debugger connection lost.
Shutting down...

Thanks,

Doug Burrell

This topic has been closed for replies.

5 replies

Markus GIRDLAND
ST Employee
May 28, 2020

Make sure wiring and the hardware aspects of your custom board is set up correctly. Do you have CubeProgrammer as a stand-alone application as well? If so, do you receive the same issue when you try to connect to CubeProgrammer stand-alone?

DBurr
DBurrAuthor
Senior
May 28, 2020

I've already been able to load the firmware onto the board using STM32CubeProgrammer stand along application so the hardware and JTAG connection appears to be working correctly.

Uwe Bonnes
Chief
May 29, 2020

STLinkv3 denies working with non-STM32 parts and is more picky to connect to STM32 parts in certain run states. If you have another debugger, try that first.

DBurr
DBurrAuthor
Senior
May 29, 2020

Are you suggesting some other type of JTAG adaptor than the ST-LinkV3? This is the only HW debugger I have. I've already verified it works along with my board since I've been able to program the board using STM32CubeProgrammer so there is some problem with STM32CubeIDE and am hoping someone here can suggest a fix.

Uwe Bonnes
Chief
May 29, 2020

First test is always to connect under reset. Expect also misbehaving cables and connectors