Skip to main content
ERhod.1
Associate II
August 5, 2021
Question

Error when programing Nucleo Board(MB1364) with 1.8V

Hi everyone, thank you for your help.

Currently I can program the stm32h723 device at the nucleo board using the ST-Link V3 with the MCU voltage set to 3V3 but cannot with the voltage set to 1V8.

I bought the STLINK-V3SET and the STLINK-V3 voltage conversion expansion board, followed the mounting steps to stack the MB1441 (STlink V3) and the MB1598 (Voltage conversion) and I am still getting the same error message when I try to program the device through the MIPI 10 connector using the Cube IDE.

This is the complete error message I get when I try to program the device:

"Failed to start GDB server

Error in initializing ST-LINK device.

Reason: (13) Unknown. Please check power and cabling to target."

Regards

Edu.

This topic has been closed for replies.

6 replies

TDK
August 6, 2021

Can you program via STM32CubeProgrammer? Does it detect the chip and voltage okay?

"If you feel a post has answered your question, please click ""Accept as Solution""."
ERhod.1
ERhod.1Author
Associate II
August 6, 2021

Yes, it worked. Thank you for the suggestion. Any idea why it works with the STM32CubeProgrammer but not with the STM32CubeIDE?

Andreas Bolsch
Lead III
August 6, 2021

Hm, I had no trouble with nucleo-h723zg and the internal STLink-V3 at VDD 1.8V (by moving JP5). Same on nucleo-h7a3zi-q, in both cases with OpenOCD.

AFAIK GDB-server internally uses OpenOCD, so you might try this directly to diagnose the problem. The cfg file I'm using is attached.

BTW: You're using a bare nucleo-board without *any* external hardware attached?

ERhod.1
ERhod.1Author
Associate II
August 6, 2021

Yes, I am using a bare nucleo board.

I will try using the OpenOCD and will give a feedback. Thank you for your suggestion.

ERhod.1
ERhod.1Author
Associate II
August 6, 2021

I tried with OpenOCD as the debug probe at the CubeIDE and got all these messages:

Open On-Chip Debugger 0.11.0-rc2+dev-00037-g4c4dbd9 (2021-02-09-13:39)

Licensed under GNU GPL v2

For bug reports, read

   http://openocd.org/doc/doxygen/bugs.html

Info : Listening on port 6666 for tcl connections

Info : Listening on port 4444 for telnet connections

Info : STLINK V3J7M2B4S1 (API v3) VID:PID 0483:374F

Info : Target voltage: 1.808417

Info : clock speed 8000 kHz

Info : stlink_dap_op_connect(connect)

Info : SWD DPIDR 0x6ba02477

Info : STM32H735ZGTx.cm7: hardware has 8 breakpoints, 4 watchpoints

Info : STM32H735ZGTx.cm7: external reset detected

Info : starting gdb server for STM32H735ZGTx.cm7 on 3333

Info : Listening on port 3333 for gdb connections

Info : accepting 'gdb' connection on tcp/3333

target halted due to debug-request, current mode: Thread

xPSR: 0x01000000 pc: 0x080005f8 msp: 0x20020000

Info : Device: STM32H72x/73x

Info : flash size probed value 1024

Info : STM32H7 flash has a single bank

Info : Bank (0) size is 1024 kb, base address is 0x08000000

Info : New GDB Connection: 1, Target STM32H735ZGTx.cm7, state: halted

Info : accepting 'gdb' connection on tcp/3333

target halted due to debug-request, current mode: Thread

xPSR: 0x01000000 pc: 0x080005f8 msp: 0x20020000

Info : New GDB Connection: 2, Target STM32H735ZGTx.cm7, state: halted

target halted due to debug-request, current mode: Thread

xPSR: 0x01000000 pc: 0x080005f8 msp: 0x20020000

Info : Padding image section 0 at 0x08001bcc with 20 bytes (bank write end alignment)

target halted due to debug-request, current mode: Thread

xPSR: 0x01000000 pc: 0x080005f8 msp: 0x20020000

shutdown command invoked

Info : dropped 'gdb' connection

shutdown command invoked

So I do not know how to interpret that. it looks like it gets halted all the time by another debug request.