Skip to main content
Visitor II
April 9, 2024
Question

Error: target voltage may be too low for reliable debugging

I have an Nucleo F401RE Board where i broke of the stlink part.

Now i try to use this stlink part to programm and debug an stm32f401cc blackpill board.

I works that i can flash my code onto the blackpill mcu (using platformio and openocd), but i always get the following error message:
Error: target voltage may be too low for reliable debugging.

If i try to start a debug session it won't work.

The STM32CubeProgrammer shows the voltage of the board 0,1V.

I connected a 3,3V pin on the blackpill to the VDD pin on the SWD header at the stlink.

Don't know what i am missing here? Maybe someone can help?

 

This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
April 9, 2024

Is the BlackPill self powered? Please diagram all the wiring, USB, etc in your proposed implementation

There might be a better place in inject power on the NUCLEO/ST-LINK stub board, you could check the schematic.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..