Skip to main content
TDK
October 29, 2019
Question

Error in UM2408 on LD1 connection

  • October 29, 2019
  • 1 reply
  • 575 views

There is an error in UM2408 regarding the connections for LD1.

In section "6.6 LEDs", it currently reads:

User LD1: a green user LED is connected to the STM32H7 I/O PB0 (SB39 ON and SB47

OFF) or PA5 (SB65 ON and SB54 OFF) corresponding to the ST Zio D13.

It should read:

User LD1: a green user LED is connected to the STM32H7 I/O PB0 (SB54 ON and SB65

OFF) or PA5 (SB65 ON and SB54 OFF) corresponding to the ST Zio D13.

https://www.st.com/resource/en/user_manual/dm00499171.pdf

This topic has been closed for replies.

1 reply

ST Technical Moderator
October 30, 2019

Hello @TDK​ ,

Thank you for reporting this error. We will correct this in the next release of UM2408.

Best Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks