Skip to main content
Visitor II
February 11, 2026
Question

Error in initializing ST-LINK device. Reason: Target not halted.

  • February 11, 2026
  • 1 reply
  • 224 views

Hello everyone, 

 

I recently bought the NUCLEO-N657X0-Q and I am trying to debug it using the ST-LINK_gdbserver.

Also this is my first development board and I don't know where to look. The data sheet and reference manual give me nothing in this regard and I am helpless. 

Here is the command line output:

$ /opt/ST/STM32CubeCLT_1.20.0/STLink-gdb-server/bin/ST-LINK_gdbserver --swd \ 
 -cp /opt/ST/STM32CubeCLT_1.20.0/STM32CubeProgrammer/bin -v -l 31 --frequency 8000 -k 


STMicroelectronics ST-LINK GDB server. Version 7.12.0
Copyright (c) 2025, STMicroelectronics. All rights reserved.

Starting server with the following options:
 Persistent Mode : Disabled
 Logging Level : 31
 Listen Port Number : 61234
 Status Refresh Delay : 15s
 Verbose Mode : Enabled
 SWD Debug : Enabled
 InitWhile : Enabled

COM frequency = 8000 kHz
Target connection mode: Under reset
Target not halted after reset. Force halt
Failed to halt target
Target not halted

Error in initializing ST-LINK device.
Reason: Target not halted.

I am on macOS Tahoe 26.2.

I have ruled out that it is due to connectivity problems because I can program the board and run software on it using the STM32CubeProgrammer and its corresponding STM32_Programmer_CLI. I can also halt the core, inspect memory, read system registers and configure peripherals. I have also not encountered anyone with a similar problem on the internet.  BOOT0 is LOW and BOOT1 is HIGH to enter development boot. The board is connected through the CN10 USB-C port and the 5V_PWR LED (LD1) is ON. Also the PWR status tricolor LED (LD4) is GREEN which indicates that the power delivery is okay.

 I got a simple blinking LED to work with basic GPIO but more complex projects require a debugger. I am deliberately avoiding the STM32CubeIDE because I do not want any hardware abstractions, but even CLion throws this exact error when I try to connect.

 

Please help me resolve this issue, I would be grateful!

 

For certainty here are more details from the STM32_Programmer_CLI:

ST-LINK SN : 003C00184142501420353451
ST-LINK FW : V3J16M8
Board : NUCLEO-N657X0-Q
Voltage : 3.28V
SWD freq : 8000 KHz
Connect mode: Normal
Reset mode : Software reset
Device ID : 0x486
Revision ID : Rev B
Device name : ST32N657
Device type : MCU
Device CPU : Cortex-M55
BL Version : --

 

Thank you in advance!

1 reply

Mike_ST
ST Technical Moderator
February 12, 2026

Hello,

I don't know about GDB server nor MacOS, but with GDB you have :

>> Target connection mode: Under reset

and with STM32CubeProgrammer_CLI, where it works:

>> Connect mode: Normal
>> Reset mode : Software reset

So based on the GDB server User Manual I would at least try to remove the -k option.

-v -l 31 --frequency 8000 -k

I don't know much more...

>> STM32CubeIDE because I do not want any hardware abstractions

You don't have to compile/call the HAL/LL libraries when you're using the CubeIDE, you can make direct register accesses as well, if that's what you mean.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.