Skip to main content
rajan2
Associate II
September 27, 2011
Question

Error in Initializing ST-Link device

Posted on September 27, 2011 at 05:06

Hi, 

Just started playing around with my STM32 discovery board, and had a problem right away. I'm using atollic trueStudio IDE and trying to load a demo project(the one in firmware package), to my microcontroller. The thing is everytime I hit debug button It shows this in console:

Starting server with the following options: 

        Persistant Mode            : Disabled 

        LogFile Name               : debug_log.txt

        Logging Level              : 1

        Listen Port Number         : 61234

        Status Refresh Delay       : 15s

        Verbose Mode               : Disabled 

        SWD Debug                  : Enabled 

Error in Initializing ST-Link device

I spent entire day searching web, if I could find a solution but no success yet. I found this page(

http://www.atollic.com/index.php/kb/3-debugging/28-kb_st_link_connection_error

) on atollic website, have followed the steps but still no luck. So these are the things which I have already tried:

- checked USB cable

- tried running ST-LINK GDB server, same error

- checked the driver installation, and updated to latest version

- no disk letter issue, st link is using G: and it is vacant

I have followed the user manual steps exactly still unsure what's wrong with my board. Any help appreciated.

#debugging #st-link-gdbserver #driver
This topic has been closed for replies.

16 replies

rouxel
Visitor II
June 6, 2012
Posted on June 06, 2012 at 15:35

Hello,

I have the same problem and i didn't find a solution, can somebody help me ?

Florent

frankmeyer9
Associate III
June 6, 2012
Posted on June 06, 2012 at 16:08

You might have not yet installed the ST-Link USB driver.

The discovery boards have one integrated, either the old version V1 (VL_Discovery), or the new version (V2, all later boards).

Usually, a ''new hardware detected'' window pops up under Windows. Just follow it (automatic installation, no access to internet required).

This drivers can also be found here:

http://www.st.com/internet/evalboard/product/251168.jsp

(down at the page, under ''SW DRIVERS''

rouxel
Visitor II
June 6, 2012
Posted on June 06, 2012 at 16:24

Thank you your response, but i don't think the driver is the problem.

 Unlike the original poster, I already ran programs on the board.While I was manipulating a DB9 connector for RS232 connection, I got a bluescreen on my computer. And since that day, the same error pop-ups everytime I try to launch a debug session :

http://image.noelshack.com/fichiers/2012/23/1338825285-cc.png

frankmeyer9
Associate III
June 6, 2012
Posted on June 06, 2012 at 16:46

Bluescreens are sometimes refered to as BSOD...

Your Windows Registry might got corrupted or partially wiped out.

I would completely remove the driver in the hardware manager, and reinstall it.

I hope you have a backup. Perhaps you are lucky, but expect more maladies.

frankmeyer9
Associate III
June 6, 2012
Posted on June 06, 2012 at 16:51

Addendum:

If you had this RS232 on a USB/RS232 adapter, you might have damaged that USB chip in your PC physically.

Often there are more than one USB host adapters in a PC. Can you try a USB port on another driver chip ?

rouxel
Visitor II
June 6, 2012
Posted on June 06, 2012 at 17:05

I tried other usb port nothing new. I even try to run the same program with an other PC and an other board, but i got the same error... If it is an error related to the code, I don't understand why, when I create a new project, I get the same problem.

Tesla DeLorean
Guru
June 6, 2012
Posted on June 06, 2012 at 18:34

If the code programmed on the STM32 is non conducive to SWD connectivity, try pulling BOOT0 High, and restart the board so it enters system loader mode.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
frankmeyer9
Associate III
June 6, 2012
Posted on June 06, 2012 at 19:56

''Error in Initializing ST-Link device

'' points to a problem with the stlink debug adapter, which is the bridge to your application, so to speak. If the host can't find the stlink, you don't have a chance to flash/debug your application.

rouxel
Visitor II
June 7, 2012
Posted on June 07, 2012 at 16:05

Thank you, I pulled BOOT0 high, it works with my coworker's board, but for me, a new error appears :

http://www.noelshack.com/2012-23-1339077525-cc2.png

If nothing get better, I'll replace the board.

frankmeyer9
Associate III
June 8, 2012
Posted on June 08, 2012 at 17:47

Well, I have some troubles to understand french error message, but it still seems that Atollics GDB server can't access the stlink.

It is certainly not impossible that the board or the stlink part is damaged.

Have you tried the STLink Utility ?

Does it show the same issue if you try the board on your co-workers PC (or any other PC, for that matter) ?

If you have some testhardware attached, better remove it.

I, for instance, had difficulties when trying to debug a stm32f4discovery with a LCD panel attached. It worked reliably only after supplying the board externally, and not via USB.